WB55: Leaving the chip in the brick after loading the stack. Very important for everyone.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-13 6:38 AM
2 years ago it happened that the controller turned to brick. I corresponded with technical support for a long time and I was offered to send the controller to the factory or representative. But since the case was a single one, I did not take advantage of this case and forgot about it.
Now there is a situation that, probably, everyone who uses this chip has, namely, that for unknown reasons it turns into a brick.
I re-read all my messages in the STM community, but to my surprise, the post in which I described the transformation into brick disappeared.
Today I have about 70 controllers with which I cannot do anything because they are not programmable.
I decided to understand the reason and found it.
The reason is well described in the post:
https://community.st.com/s/feed/0D53W000010si7oSAA?t=1676280731376
But for all this time, not a single STM employee has given a clear explanation of why this is happening.
The question is simple: why sometimes, after loading the stack, the chip register SFSA = 0?
After all, because of this, the chip turns into a brick.
I lost some money to buy the chips, but I lost a lot more because I couldn't sell my final product.
How long will STM keep silent about this problem?
None of the ERRATAs describe this case.
It turns out that STM does not give a damn about its consumers?
If the official representatives do not answer this question, I will raise a storm on the Internet about the quality of the chips and the sabotage of employees in front of consumers.
Vyacheslav : Bluetooth SIG Id is "LVI Cо."
Solved! Go to Solution.
- Labels:
-
STM32WB series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-17 12:31 AM
I solved my problem.
Thanks to the topic
Now I can restore chips.
The procedure is as follows:
Using STM32CubeProgrammer via ST-Link.
- "User Configuration" option bytes bring it to the factory initial state.
- write 0x00008000 to the PWR_CR4 register. (start CPU2)
-wait 5 seconds after which the remaining registers of options bytes dependent on CPU2 return to safe boot state.
- hard reset chip.
Now chip in factory default state.
But it works only if FUS V1.1.0 or higher version.
If a FUS version lower than V1.1.0 is running, then, no recovery is possible at this point. (AN5185 page 10)
Regards,
Vyacheslav.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-13 7:11 AM
Is it possible that this is your old thread?
Please keep in mind, that the community is a place for questions where users can benefit from the experiences of other users. Now that @Remi QUINTIN​ has helped you before, perhaps he will be so kind again?
Regards
/Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-13 7:24 AM
Thanks for the quick response.
But this is not the thread.
By the way, the problem was not solved in the specified thread either, so we still use the version of SDK 1.11 in the old device only because of the indicated problem.
And the thread about which I spoke, where the states of the register were indicated many times - it does not exist.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-16 3:36 AM
I have the same problem. During the erasure of all memory, sometimes the chip turns into a brick. Through st link, you can only read the memory. It is impossible to change anything. Sometimes this happens when the stack is loaded. Indeed the ship register SFS A = 0
I have a lot of such chips. I don't know what to do with them now.
Best regards
TheRom
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-16 10:31 AM
Hello,
Can you share the value of SBRV option byte? And which FUS version did you used?
Best Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-16 11:49 AM
Hello, Remy.
The default FUS in clear chip is 1.2.0
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
ST-LINK SN : 53FF6A064975524934100567
ST-LINK FW : V2J36S7
Board : --
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x58004020
Size : 96 Bytes
±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0%
џџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџџ 100%±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 50%
ÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸÑŸ 100%
Bank : 0x01
Address : 0x58004080
Size : 8 Bytes
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
User Configuration:
nBOOT0 : 0x1 (nBOOT0=1 Boot from main Flash)
nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
nSWBOOT0 : 0x1 (BOOT0 taken from PH3/BOOT0 pin)
SRAM2RST : 0x0 (SRAM2 erased when a system reset occurs)
SRAM2PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDGSW : 0x1 (Software window watchdog)
IWDGSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDGSW : 0x1 (Software independent watchdog)
IPCCDBA : 0x0 (0x0)
Security Configuration Option bytes - 1:
ESE : 0x1 (Security enabled)
PCROP Protection:
PCROP1A_STRT : 0x1FF (0x80FF800)
PCROP1A_END : 0x0 (0x8000800)
PCROP_RDP : 0x1 (PCROP zone is erased when RDP is decreased)
PCROP1B_STRT : 0x1FF (0x80FF800)
PCROP1B_END : 0x0 (0x8000800)
Write Protection:
WRP1A_STRT : 0xFF (0x80FF000)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x80FF000)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1
Security Configuration Option bytes - 2:
SFSA : 0x0 (0x8000000)
FSD : 0x0 (System and Flash secure)
DDS : 0x1 (CPU2 debug access disabled)
C2OPT : 0x1 (SBRV will address Flash)
NBRSD : 0x0 (SRAM2b is secure)
SNBRSA : 0x0 (0x20038000)
BRSD : 0x0 (SRAM2a is secure)
SBRSA : 0x0 (0x20030000)
SBRV : 0x3FC00 (0x20000000)
Regards,
Vyacheslav.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-17 12:31 AM
I solved my problem.
Thanks to the topic
Now I can restore chips.
The procedure is as follows:
Using STM32CubeProgrammer via ST-Link.
- "User Configuration" option bytes bring it to the factory initial state.
- write 0x00008000 to the PWR_CR4 register. (start CPU2)
-wait 5 seconds after which the remaining registers of options bytes dependent on CPU2 return to safe boot state.
- hard reset chip.
Now chip in factory default state.
But it works only if FUS V1.1.0 or higher version.
If a FUS version lower than V1.1.0 is running, then, no recovery is possible at this point. (AN5185 page 10)
Regards,
Vyacheslav.