cancel
Showing results for 
Search instead for 
Did you mean: 

WB55: A friend node can connect up to 6 LPNs at most

DL_Weng
Associate II

Hi,

DL_Weng_0-1733725418160.png

 

The correspondence between friend nodes and LPNs in the ST official website description states that a friend node can connect up to 6 LPNs at most. Other chips can connect more LPN nodes with one friend node. Has ST optimized in this area?

Thanks,

DL_Weng

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @DL_Weng 

The LPN/friend association is limited by the 1KB SRAM available and the Radio Time that it take. That’s why is recomanded to Connect a maximum of 6 LPN to the same end friend node.

Best Regards. 
STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @DL_Weng 

The LPN/friend association is limited by the 1KB SRAM available and the Radio Time that it take. That’s why is recomanded to Connect a maximum of 6 LPN to the same end friend node.

Best Regards. 
STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.