2024-03-02 04:13 PM
Using Nucleo-WB55 and I call the above command. I put a break point and can see then later that I call UTIL_SEQ_SetTask with the same mask HOWEVER I never go back into my function. Can anyone tell me what I am doing wrong?
2024-04-18 05:45 AM
Hello @SWenn.1
Can you give more details about your project, the implementation that you are using and your project if possible.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.