2024-11-06 12:28 AM - last edited on 2024-11-06 02:10 AM by Andrew Neil
Hi,
I just want to make sure that it is possible Using STM32WLE5 SUBGHZ IN HIGH-POWER MODE (22 DBM) , higher frequency band , WITH THE INTERNAL LDO ? (without the internal SMPS )
I am asking because i see in the CUBE-MX under the tools tab that there is no option to select "high-power" when selecting "SMPS OFF"
Thank You,
Viola
2024-11-06 02:03 AM
Hello @viola
As you can see on the chapter 4.3.3 of the RM0461, the transmitter for high output power does not need SMPS to be configured :
For the CubeMX part, can you please give more details (how to reproduce).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-06 02:52 AM
Hi ,
As you can see in the picture below , I dont have the option for "high power" when "SMPS" is OFF