2024-01-19 10:02 AM
Hello guys!
I'm working with STM32WL series using the LoRa application, for that the RTC must be in binary mode.
However, I need the calendar and timestamp for my project, which implies that I need to use BCD mode.
I'm aware that the RTC3 has the mixed mode, however, whenever I tried using it, the whole project stopped working.
I've been reading the AN4759, and the posts about it in the community, but I have some doubts about the solution.
LoRa uses the alarm A, which requires the subseconds alarm, and I know that the calendar doesn't work in binary mode, but can I activate somehow by software the calendar and timestamp still in binary mode? (if so, how and where in the code?)
Other thing, while using the mixed mode, what I have to do to make it work like in binary mode but with the calendar? Like, I saw that I might have to transform binary date to BCD, is it necessary? If so, I'm confused how and where in the code I do this. Also I need to adjust the alarm A again, right? What do I have to correct in this case?
Thanks in advance!
2024-03-04 08:45 AM
Hello @FPicc.1
RTC is indeed reserved for SUBGHz, if you want to get a calendar you can use the time system Offred by the stm32_systime (available in utilities) which provides the time feature based on RTC, please have a look. With it you can dynamically set the time, get the time and maintain it to configure a calendar (main APIs and how to use described in AN5406).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-04 11:31 AM
Thanks for the reply @STTwo-32 , but would I be able to update the timestamp value of the SysTimeMkTime() function, for example, every second?
Can I get a continuous timestamp from these functions?
2024-03-18 02:01 PM - edited 2024-03-18 02:02 PM
I am stuck with the same situation and the closest I got was to realize that the STM32duino Lorawan wrapper (apparently also provided by ST) seems to use RTC in mixed mode by default and uses Alarm B for the Lorawan stack timing.
There is an example with a calendar alarm and Lorawan, so it seems to work.
Let me know if you got it to work!
2025-02-10 04:48 AM
Hi @FPicc.1,
Have you found a solution for this? I also need to use the RTC in both binary and BCD modes for timestamps, but when I enable RTC_BINARY_MIX, LoRa stops working.
I’d appreciate it if you could share any progress or insights you’ve made on this issue.
Thanks in advance!
Best Regards,
Samidha