cancel
Showing results for 
Search instead for 
Did you mean: 

Using I-CUBE-LRWAN in a separate project generated with CUBE-MX

Szcz3pan
Associate

Hi,
Is it possible to import files from I-CUBE-LRWAN package to a new project generated with MX? From the info I've found so far I know there is no way to import it automatically with Cube MX and I have to transfer them manually but I'm not sure which ones and how to link them later.

I'm using b-l072z-lrwan1 board and would like to have the functionality of the "end-node" example from I-CUBE-LRWAN package.

How should I go about this?

1 REPLY 1
STTwo-32
ST Employee

Hello @Szcz3pan and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you start from the "LoRaWAN_End_Node" example on the I-CUBE-LRWAN package. Then, you can do the necessary changes to adapt it to your needs. You can also take a look on this playlist specially the videos Number 6 and 7 to understand more about the package and the End_Node application.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.