2023-12-10 08:20 AM
Hi,
Is it possible to import files from I-CUBE-LRWAN package to a new project generated with MX? From the info I've found so far I know there is no way to import it automatically with Cube MX and I have to transfer them manually but I'm not sure which ones and how to link them later.
I'm using b-l072z-lrwan1 board and would like to have the functionality of the "end-node" example from I-CUBE-LRWAN package.
How should I go about this?
2023-12-11 12:43 AM
Hello @Szcz3pan and welcome to the ST Community 😊.
I suggest you start from the "LoRaWAN_End_Node" example on the I-CUBE-LRWAN package. Then, you can do the necessary changes to adapt it to your needs. You can also take a look on this playlist specially the videos Number 6 and 7 to understand more about the package and the End_Node application.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.