2025-01-17 8:09 AM - edited 2025-01-17 8:09 AM
We have been running into an issue on brand new custom hardware with the STM32wb55 chip that when we perform a FUS and BLE stack update using the stm_programmer CLI tool we need to perform a full power removal and apply before the BLE stack will actually work. When we run our tools to provision a board after the wireless stack upgrade is done we gave it the start stack command and when we boot into our application the cpu2 is failing to init. To recover from this we need to completely remove power and re apply for it to work.
Does the wireless stack upgrade require a full power cycle to complete. We are using the command line tools connect under reset to try and trigger a reset of cpu2 but it does not.
Solved! Go to Solution.
2025-01-22 11:46 PM
Hello,
please check chapter 2.3 Empty check in STM32WB55 reference manual
"...A power reset or setting the OBL_LAUNCH bit in FLASH_CR register is needed to clear this flag after programming of a virgin device..."
Setting option bytes during your initial reset should prevent need for power reset during our initial programming.
Best regards,
Lubos
2025-01-22 11:46 PM
Hello,
please check chapter 2.3 Empty check in STM32WB55 reference manual
"...A power reset or setting the OBL_LAUNCH bit in FLASH_CR register is needed to clear this flag after programming of a virgin device..."
Setting option bytes during your initial reset should prevent need for power reset during our initial programming.
Best regards,
Lubos