The SPI data length is set to 8 bits, but the receive data buffer is 16 bits
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-23 4:31 AM
In STM32WLE5JC MCU, the SPI data length is set to 8 bits, and the corresponding receiving FIFO is also set to 8 bits, but the final receiving and sending data is 16 bits.
1. SPI-CR2 registers during transmission are as follows:
It can be seen from the figure that CR2 is 0x1708, the threshold of FIFO is set to 8 bits, but the data length of DR is 16 bits: 0x0130
2. the CR2 register in 2.STM32WL is described as follows:
- Labels:
-
Documentation
-
SPI
-
STM32WL series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-23 4:47 AM
Ok, but you understand the debugger is invasive, right?
It forcibly reads, in a wide fashion, and changes the internal state of the peripheral.
It doesn't care about the FIFO depth, or data ready. The data in DR is undefined in the empty case.
Up vote any posts that you find helpful, it shows what's working..