cancel
Showing results for 
Search instead for 
Did you mean: 

Sub-GHz and ADC DMA integration errors

MichaelMor
Associate II

Hi All,

I'm using STM32WL55JC board which include Sub-GHz, ADC and DMA peripherals (and many more of course)
I run "ping pong" example to create Sub-GHz communication sucssfully, also run "ADC_SingleConversion_TriggerTimer_DMA" and changed to circular mode (DMA) I saw buffer changing variables according to ADC result.
I configured ADC and DMA at "ping pong" example exactly as they configured at ADC example, and start via HAL_ADC_Start_DMA() command the buffer result is written only once, then program start Sub_GHz routine of RX-TX and the buffer results stuck and doesn't change.
what can be the reason?

adding some pictures from ping-pong - ADC DMA configuration
I'll appreciate your help!

3 REPLIES 3
mrox
Associate II

I think you should provide the code, instead of the screenshots.

MichaelMor
Associate II

ON SUB-GHZ-INIT ADC_DMA START

  ******************************************************************************
  * @file    subghz_phy_app.c
  * @author  MCD Application Team
  * @brief   Application of the SubGHz_Phy Middleware
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2021 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "platform.h"
#include "sys_app.h"
#include "subghz_phy_app.h"
#include "radio.h"
#include "adc.h"
#include "stdio.h"
#include "stdlib.h"
#include "ctype.h"

/* USER CODE BEGIN Includes */
#include "stm32_timer.h"
#include "stm32_seq.h"
#include "utilities_def.h"
#include "app_version.h"
#include "subghz_phy_version.h"
/* USER CODE END Includes */

/* External variables ---------------------------------------------------------*/
/* USER CODE BEGIN EV */

/* USER CODE END EV */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
typedef enum
{
  RX,
  RX_TIMEOUT,
  RX_ERROR,
  TX,
  TX_TIMEOUT,
} States_t;

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* Configurations */
/*Timeout*/
#define RX_TIMEOUT_VALUE              3000
#define TX_TIMEOUT_VALUE              3000
#define PWMSettleTime   1000 //one second
/* PING string*/

#define SYNC "SYNC"
#define SYNCRESPONSE "SYNC2 DONE"

#define ID "NODE1B"
#define COMMA ","

/*Size of the payload to be sent*/
/* Size must be greater of equal the PING and PONG*/
#define MAX_APP_BUFFER_SIZE          255
#if (PAYLOAD_LEN > MAX_APP_BUFFER_SIZE)
#error PAYLOAD_LEN must be less or equal than MAX_APP_BUFFER_SIZE
#endif /* (PAYLOAD_LEN > MAX_APP_BUFFER_SIZE) */
/* wait for remote to be in Rx, before sending a Tx frame*/
#define RX_TIME_MARGIN                200
/* Afc bandwidth in Hz */
#define FSK_AFC_BANDWIDTH             83333
/* LED blink Period*/
#define LED_PERIOD_MS                 200

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */
static void MX_DMA_Init(void);
/* Private variables ---------------------------------------------------------*/
/* Radio events function pointer */
static RadioEvents_t RadioEvents;

/* USER CODE BEGIN PV */
/*Ping Pong FSM states */
static States_t State = RX;
/* App Rx Buffer*/
static uint8_t BufferRx[MAX_APP_BUFFER_SIZE];
/* App Tx Buffer*/
static uint8_t BufferTx[MAX_APP_BUFFER_SIZE];
/* Last  Received Buffer Size*/
uint16_t RxBufferSize = 0;
/* Last  Received packer Rssi*/
int8_t RssiValue = 0;
/* Last  Received packer SNR (in Lora modulation)*/
int8_t SnrValue = 0;
/* Led Timers objects*/
static UTIL_TIMER_Object_t timerLed;
/* device state. Master: true, Slave: false*/
bool isMaster = true;
/* random delay to make sure 2 devices will sync*/
/* the closest the random delays are, the longer it will
   take for the devices to sync when started simultaneously*/
static int32_t random_delay;

 


extern ADC_HandleTypeDef hadc;
#define ADC_CONVERTED_DATA_BUFFER_SIZE   ((uint32_t)  200 )
__IO   uint16_t   aADCxConvertedData[ADC_CONVERTED_DATA_BUFFER_SIZE]; /* ADC group regular conversion data (array of data) */


/* Variables for ADC conversion data */
//__IO   uint16_t   uhADCxConvertedData = VAR_CONVERTED_DATA_INIT_VALUE; /* ADC group regular conversion data */
#define DIGITAL_SCALE_12BITS             ((uint32_t) 0xFFF)

/* Init variable out of ADC expected conversion data range */
#define VAR_CONVERTED_DATA_INIT_VALUE    (DIGITAL_SCALE_12BITS + 1)
/* Variables for ADC conversion data computation to physical values */
uint16_t   uhADCxConvertedData_Voltage_mVolt [ADC_CONVERTED_DATA_BUFFER_SIZE];  /* Value of voltage calculated from ADC conversion data (unit: mV) */
unsigned long value = 0;

#define NumberOfPeaksRequired   ((uint32_t)  3)
volatile uint16_t MaxPeak = 0 ;
volatile uint16_t ArrayMaxPeakmV [NumberOfPeaksRequired];
volatile uint16_t i = 0;

volatile uint16_t NumberOfMaxPeak = 0;
volatile double AverageMaxPeakmV = 0;
__IO   uint16_t   uhADCxConvertedData = VAR_CONVERTED_DATA_INIT_VALUE; /* ADC group regular conversion data */
int8_t IDNumber = 2;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
/*!
 * @brief Function to be executed on Radio Tx Done event
 */
static void OnTxDone(void);

/**
  * @brief Function to be executed on Radio Rx Done event
  * @PAram  payload ptr of buffer received
  * @PAram  size buffer size
  * @PAram  rssi
  * @PAram  LoraSnr_FskCfo
  */
static void OnRxDone(uint8_t *payload, uint16_t size, int16_t rssi, int8_t LoraSnr_FskCfo);

/**
  * @brief Function executed on Radio Tx Timeout event
  */
static void OnTxTimeout(void);

/**
  * @brief Function executed on Radio Rx Timeout event
  */
static void OnRxTimeout(void);

/**
  * @brief Function executed on Radio Rx Error event
  */
static void OnRxError(void);

/* USER CODE BEGIN PFP */
/**
  * @brief  Function executed on when led timer elapses
  * @PAram  context ptr of LED context
  */
static void OnledEvent(void *context);

/**
  * @brief PingPong state machine implementation
  */
static void PingPong_Process(void);

bool isIDPresentInBuffer(const char *id);
/* USER CODE END PFP */

/* Exported functions ---------------------------------------------------------*/
void SubghzApp_Init(void)
{
  /* USER CODE BEGIN SubghzApp_Init_1 */

MX_ADC_Init();
MX_DMA_Init();
HAL_ADC_Start_DMA(&hadc,
                                                   (uint32_t *)aADCxConvertedData,
                                                 ADC_CONVERTED_DATA_BUFFER_SIZE
                                                );
  APP_LOG(TS_OFF, VLEVEL_M, "\n\rPING PONG\n\r");
  /* Get SubGHY_Phy APP version*/
  APP_LOG(TS_OFF, VLEVEL_M, "APPLICATION_VERSION: V%X.%X.%X\r\n",
          (uint8_t)(APP_VERSION_MAIN),
          (uint8_t)(APP_VERSION_SUB1),
          (uint8_t)(APP_VERSION_SUB2));

  /* Get MW SubGhz_Phy info */
  APP_LOG(TS_OFF, VLEVEL_M, "MW_RADIO_VERSION:    V%X.%X.%X\r\n",
          (uint8_t)(SUBGHZ_PHY_VERSION_MAIN),
          (uint8_t)(SUBGHZ_PHY_VERSION_SUB1),
          (uint8_t)(SUBGHZ_PHY_VERSION_SUB2));

  /* Led Timers*/
  UTIL_TIMER_Create(&timerLed, LED_PERIOD_MS, UTIL_TIMER_ONESHOT, OnledEvent, NULL);
  UTIL_TIMER_Start(&timerLed);
  /* USER CODE END SubghzApp_Init_1 */

  /* Radio initialization */
  RadioEvents.TxDone = OnTxDone;
  RadioEvents.RxDone = OnRxDone;
  RadioEvents.TxTimeout = OnTxTimeout;
  RadioEvents.RxTimeout = OnRxTimeout;
  RadioEvents.RxError = OnRxError;

  Radio.Init(&RadioEvents);

  /* USER CODE BEGIN SubghzApp_Init_2 */
  /*calculate random delay for synchronization*/
  random_delay = (Radio.Random()) >> 22; /*10bits random e.g. from 0 to 1023 ms*/

  /* Radio Set frequency */
  Radio.SetChannel(RF_FREQUENCY);

  /* Radio configuration */
#if ((USE_MODEM_LORA == 1) && (USE_MODEM_FSK == 0))
  APP_LOG(TS_OFF, VLEVEL_M, "---------------\n\r");
  APP_LOG(TS_OFF, VLEVEL_M, "LORA_MODULATION\n\r");
  APP_LOG(TS_OFF, VLEVEL_M, "LORA_BW=%d kHz\n\r", (1 << LORA_BANDWIDTH) * 125);
  APP_LOG(TS_OFF, VLEVEL_M, "LORA_SF=%d\n\r", LORA_SPREADING_FACTOR);

  Radio.SetTxConfig(MODEM_LORA, 22, 0, LORA_BANDWIDTH,
                    LORA_SPREADING_FACTOR, LORA_CODINGRATE,
                    LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,
                    true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);

  Radio.SetRxConfig(MODEM_LORA, LORA_BANDWIDTH, LORA_SPREADING_FACTOR,
                    LORA_CODINGRATE, 0, LORA_PREAMBLE_LENGTH,
                    LORA_SYMBOL_TIMEOUT, LORA_FIX_LENGTH_PAYLOAD_ON,
                    0, true, 0, 0, LORA_IQ_INVERSION_ON, true);

  Radio.SetMaxPayloadLength(MODEM_LORA, MAX_APP_BUFFER_SIZE);

#elif ((USE_MODEM_LORA == 0) && (USE_MODEM_FSK == 1))
  APP_LOG(TS_OFF, VLEVEL_M, "---------------\n\r");
  APP_LOG(TS_OFF, VLEVEL_M, "FSK_MODULATION\n\r");
  APP_LOG(TS_OFF, VLEVEL_M, "FSK_BW=%d Hz\n\r", FSK_BANDWIDTH);
  APP_LOG(TS_OFF, VLEVEL_M, "FSK_DR=%d bits/s\n\r", FSK_DATARATE);

  Radio.SetTxConfig(MODEM_FSK, TX_OUTPUT_POWER, FSK_FDEV, 0,
                    FSK_DATARATE, 0,
                    FSK_PREAMBLE_LENGTH, FSK_FIX_LENGTH_PAYLOAD_ON,
                    true, 0, 0, 0, TX_TIMEOUT_VALUE);

  Radio.SetRxConfig(MODEM_FSK, FSK_BANDWIDTH, FSK_DATARATE,
                    0, FSK_AFC_BANDWIDTH, FSK_PREAMBLE_LENGTH,
                    0, FSK_FIX_LENGTH_PAYLOAD_ON, 0, true,
                    0, 0, false, true);

  Radio.SetMaxPayloadLength(MODEM_FSK, MAX_APP_BUFFER_SIZE);

#else
#error "Please define a modulation in the subghz_phy_app.h file."
#endif /* USE_MODEM_LORA | USE_MODEM_FSK */

  /*fills tx buffer*/
  //memset(BufferTx, 0x0, MAX_APP_BUFFER_SIZE);

  APP_LOG(TS_ON, VLEVEL_L, "rand=%d\n\r", random_delay);
  /*starts reception*/
  Radio.Rx(RX_TIMEOUT_VALUE + random_delay);

  /*register task to to be run in while(1) after Radio IT*/
  UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), UTIL_SEQ_RFU, PingPong_Process);
  /* USER CODE END SubghzApp_Init_2 */
}

/* USER CODE BEGIN EF */

/* USER CODE END EF */

/* Private functions ---------------------------------------------------------*/
static void OnTxDone(void)
{
  /* USER CODE BEGIN OnTxDone */
  APP_LOG(TS_ON, VLEVEL_L, "OnTxDone\n\r");
  /* Update the State of the FSM*/
  State = TX;
  /* Run PingPong process in background*/
  UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
  /* USER CODE END OnTxDone */
}

static void OnRxDone(uint8_t *payload, uint16_t size, int16_t rssi, int8_t LoraSnr_FskCfo)
{
  /* USER CODE BEGIN OnRxDone */

  APP_LOG(TS_ON, VLEVEL_L, "OnRxDone\n\r");
#if ((USE_MODEM_LORA == 1) && (USE_MODEM_FSK == 0))
  APP_LOG(TS_ON, VLEVEL_L, "I'm $ %s $  Recieved this data $ %s $ RssiValue=%d dBm, SnrValue=%ddB\n\r", ID ,  BufferRx ,  rssi, LoraSnr_FskCfo);  /* Record payload Signal to noise ratio in Lora*/
  SnrValue = LoraSnr_FskCfo;
#endif /* USE_MODEM_LORA | USE_MODEM_FSK */
#if ((USE_MODEM_LORA == 0) && (USE_MODEM_FSK == 1))
  APP_LOG(TS_ON, VLEVEL_L, "RssiValue=%d dBm, Cfo=%dkHz\n\r", rssi, LoraSnr_FskCfo);
  SnrValue = 0; /*not applicable in GFSK*/
#endif /* USE_MODEM_LORA | USE_MODEM_FSK */
  /* Update the State of the FSM*/
  State = RX;
  /* Clear BufferRx*/
  memset(BufferRx, 0, MAX_APP_BUFFER_SIZE);
  /* Record payload size*/
  RxBufferSize = size;
  if (RxBufferSize <= MAX_APP_BUFFER_SIZE)
  {
    memcpy(BufferRx, payload, RxBufferSize);
  }
  /* Record Received Signal Strength*/
  RssiValue = rssi;
  /* Record payload content*/
  APP_LOG(TS_ON, VLEVEL_H, "payload. size=%d \n\r", size);
  for (int32_t i = 0; i < PAYLOAD_LEN; i++)
  {
    APP_LOG(TS_OFF, VLEVEL_H, "%02X", BufferRx[i]);
    if (i % 16 == 15)
    {
      APP_LOG(TS_OFF, VLEVEL_H, "\n\r");
    }
  }
  APP_LOG(TS_OFF, VLEVEL_H, "\n\r");
  /* Run PingPong process in background*/
  UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
  /* USER CODE END OnRxDone */
}

static void OnTxTimeout(void)
{
  /* USER CODE BEGIN OnTxTimeout */
  APP_LOG(TS_ON, VLEVEL_L, "OnTxTimeout\n\r");
  /* Update the State of the FSM*/
  State = TX_TIMEOUT;
  /* Run PingPong process in background*/
  UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
  /* USER CODE END OnTxTimeout */
}

static void OnRxTimeout(void)
{
  /* USER CODE BEGIN OnRxTimeout */
  APP_LOG(TS_ON, VLEVEL_L, "OnRxTimeout\n\r");
  /* Update the State of the FSM*/
  State = RX_TIMEOUT;
  /* Run PingPong process in background*/
  UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
  /* USER CODE END OnRxTimeout */
}

static void OnRxError(void)
{
  /* USER CODE BEGIN OnRxError */
  APP_LOG(TS_ON, VLEVEL_L, "OnRxError\n\r");
  /* Update the State of the FSM*/
  State = RX_ERROR;
  /* Run PingPong process in background*/
  UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
  /* USER CODE END OnRxError */
}

/* USER CODE BEGIN PrFD */
static void PingPong_Process(void)
{
  Radio.Sleep();

  switch (State)
  {
    case RX:

        if (RxBufferSize > 0)
          {
            if (strncmp((const char *)BufferRx, SYNC, sizeof(4)) == 0)
            {


    // Search for ID in the line
                // SOME CODE TBD 


            }

            else if (strncmp((const char *)BufferRx, ID, sizeof(ID) - 1 ) == 0)
            {

             for (i = 0 ; i <= ADC_CONVERTED_DATA_BUFFER_SIZE ; i++ )
                               {
                                    //Search for the max peak value
                                    if (MaxPeak < aADCxConvertedData[i] )
                                    {
                                      //Insert peak value to
                                        MaxPeak = aADCxConvertedData[i];
                                  }
                                }

              UTIL_TIMER_Stop(&timerLed);
              /* switch off red led */
              HAL_GPIO_WritePin(LED3_GPIO_Port, LED3_Pin, GPIO_PIN_RESET); /* LED_RED */
              /* slave toggles green led */
              HAL_GPIO_TogglePin(LED2_GPIO_Port, LED2_Pin); /* LED_GREEN */
              /* Add delay between RX and TX */
              //HAL_Delay(Radio.GetWakeupTime() );//HAL_Delay(Radio.GetWakeupTime() + RX_TIME_MARGIN);
              /*slave sends PONG*/

              APP_LOG(TS_ON, VLEVEL_L, "Slave  Tx start\n\r");
              
              APP_LOG(TS_ON, VLEVEL_L,
                                 "Yay you call me %s So take my data  %d \n \r" ,(const char *) ID ,MaxPeak ,
                                 "\n\r");
              memcpy(BufferTx, ID, sizeof(ID));

              sprintf(BufferTx, "%s%s%d",ID , COMMA , MaxPeak);

              Radio.Send(BufferTx, PAYLOAD_LEN);

              //NVIC_SystemReset();
            }

            else /* valid reception but not a PING as expected */
            {
              APP_LOG(TS_ON, VLEVEL_L, "No this node, I received the following address of node %s\n\r" , (const char *)BufferRx);
              Radio.Rx(RX_TIMEOUT_VALUE);
            }
        }
        break;
    case TX:
      APP_LOG(TS_ON, VLEVEL_L, "Rx start\n\r");
      Radio.Rx(RX_TIMEOUT_VALUE);
      break;
    case RX_TIMEOUT:
    case RX_ERROR:

        APP_LOG(TS_ON, VLEVEL_L, "Slave Rx start\n\r");
        Radio.Rx(RX_TIMEOUT_VALUE);

      break;
    case TX_TIMEOUT:
      APP_LOG(TS_ON, VLEVEL_L, "Slave Rx start\n\r");
      Radio.Rx(RX_TIMEOUT_VALUE);
      break;
    default:
      break;
  }
}

 

static void MX_DMA_Init(void)
{

  /* DMA controller clock enable */
  __HAL_RCC_DMAMUX1_CLK_ENABLE();
  __HAL_RCC_DMA1_CLK_ENABLE();

  /* DMA interrupt init */
  /* DMA1_Channel1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}
static void OnledEvent(void *context)
{
  HAL_GPIO_TogglePin(LED2_GPIO_Port, LED2_Pin); /* LED_GREEN */
  HAL_GPIO_TogglePin(LED3_GPIO_Port, LED3_Pin); /* LED_RED */
  UTIL_TIMER_Start(&timerLed);
}

MichaelMor
Associate II

Short explanation:
I have 2 boards, I want that every board will start ADC and measure specific channel and configured this channel, the channel initialize at "subghz_phy_app.c"(the code above)  and also start ADC_DMA at SubghzApp_Init()
from buffer of 200 ADC values I'm looking for max value and send it Sub-GHz, after sending it I want to find new max from new buffer ADC results, but I always get the same value (although I change ADCin via external P.S.)
meaning that buffer values doesn't change