cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WLE5JCI6 RX Sensitivty

viola
Associate III

Hi ,

 

is it possible to get the RX sensitivity of the STM32WLE5JCI6 in other LORA conditions then mentioned in the Datasheet ?

 

our LORA parameters are:

PER=1%

BW= 20.8Khz to 125Khz

SF= 7  to 11

split RF paths for RX and TX using RF SWITCH

 

Thank you,

Viola

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @viola 

To get such a data, you have to do the tests your self or contact one of our FAEs or marketing agent so they maybe can do it for you or give it to you if they have it from other tests that have been made.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @viola 

To get such a data, you have to do the tests your self or contact one of our FAEs or marketing agent so they maybe can do it for you or give it to you if they have it from other tests that have been made.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.