2024-10-29 09:15 PM
Hi ,
is it possible to get the RX sensitivity of the STM32WLE5JCI6 in other LORA conditions then mentioned in the Datasheet ?
our LORA parameters are:
PER=1%
BW= 20.8Khz to 125Khz
SF= 7 to 11
split RF paths for RX and TX using RF SWITCH
Thank you,
Viola
Solved! Go to Solution.
2024-10-29 09:48 PM
Hello @viola
To get such a data, you have to do the tests your self or contact one of our FAEs or marketing agent so they maybe can do it for you or give it to you if they have it from other tests that have been made.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-29 09:48 PM
Hello @viola
To get such a data, you have to do the tests your self or contact one of our FAEs or marketing agent so they maybe can do it for you or give it to you if they have it from other tests that have been made.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.