cancel
Showing results for 
Search instead for 
Did you mean: 

stm32wle5cc end_node example project

MWoło.1
Associate II

I try to create end_node project for stm32wl5cc uC, but for unkonw reason to me it is impossible

0693W000007EQeDQAW.png 

"End_Node" option is inaccessible (grey).

In LoRaWAN_End_Node example it is available.

Ho to do this in Cube Ide.

When I try to import project from NUCLEO-WL55JC I can't change uC type to stm32wle5cc

0693W000007EQeIQAW.png 

Mcu and Board It's also grey.

3 REPLIES 3
MSai
Associate II

Even i am facing Same issue

RL20
Associate

any luck solving the problem?

MWoło.1
Associate II

Hi RL20,

not so far. Someone suggest me to take existing one in Nucleo. So I created project for my uC model and just copied from Nucleo what I needed. In this approach cube mx configure soft showing something not related. Partially somethings works. I can't join to tan ;(.

Regards