2022-06-01 2:00 PM
Hi there,
I am using an STM32WLE with an input voltage range of 2 - 3.3V. It will eventually be powered by a lithium coin cell, but I am currently using a benchtop power supply. The datasheet states that both the MCU and the radio should function down to 1.8V, and my testing has confirmed this. However, I am finding that at voltages lower than 2.15V the MCU becomes unresponsive after entering Standby mode. Here are some of the behaviours I have observed at VDD < 2.15V:
The code functions as expected when the voltage is above 2.15V, and enters and exits standby with no issues.
Any clues as to what could be going on would be greatly appreciated.
Thanks,
Rebecca
Solved! Go to Solution.
2022-06-01 5:45 PM
Hi all,
Turns out it was an issue between the seat and the steering wheel. I was looking at an updated schematic that used a pin for a different function, so my PU/PD resistors were set incorrectly. The MCU now enters and exits Standby mode correctly all the way down to 1.85V.
Thanks,
Rebecca
2022-06-01 3:24 PM
The same thing as in the other topic - show the code, which enters the low-power mode and configures wake-up features.
2022-06-01 3:51 PM
Hi @Piranha ,
Here is my standby_begin() function:
void standby_begin(void)
{
// Keep SRAM2
PWR->CR3 |= PWR_CR3_RRS;
// Enable WKUP1 pin PA0
PWR->CR3 |= PWR_CR3_EWUP1;
PWR->CR4 &= ~PWR_CR4_WP1; // Rising edge
// Set SLEEPDEEP bit
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
// Set to enter standby
PWR->CR1 &= ~PWR_CR1_LPMS;
PWR->CR1 |= PWR_LOWPOWERMODE_STANDBY;
// Change to periodic sampling of VDD
PWR->CR3 |= PWR_CR3_ULPEN;
// Wait for radio to finish (if not under reset)
if (!(RCC->CSR & RCC_CSR_RFRST))
{
while((PWR->SR2 & PWR_SR2_RFBUSYMS) && (PWR->SR2 & PWR_SR2_RFBUSYS));
// Shutdown radio
RCC->CSR |= RCC_CSR_RFRST;
}
// Clear wake up flags
PWR->SCR |= 0x4907; // Clear all flags
// Set all GPIO to input
GPIOA->MODER = 0x00;
GPIOB->MODER = 0x00;
GPIOC->MODER = 0x00;
// Set all GPIO to pull down except LEDs, ADC input, SWDIO, OSC32, WKUP1
GPIOA->PUPDR = 0xA556AAA4; // 1010 0101 0101 1010 1010 1010 1010 0100
GPIOB->PUPDR = 0xAAA95AAA; // 1010 1010 1010 1001 0101 1010 1010 1010
GPIOC->PUPDR = 0x0AAAAAAA;
// Use PWR PU/PD instead of GPIOx
// PWR->PDCRA = 0xD3F4; // 1101 0011 1111 0100
// PWR->PDCRB = 0x1035; // 0001 0000 0011 0101
// PWR->PDCRC = 0x3FFF; // 0011 1111 1111 1111
// PWR->PUCRA = 0x2C0A; // 0010 1100 0000 1010
// PWR->PUCRB = 0x01C0; // 0000 0001 1100 0000
// PWR->PUCRC = 0x0000;
//
// GPIOA->PUPDR = 0x00;
// GPIOB->PUPDR = 0x00;
// GPIOC->PUPDR = 0x00;
// PWR->CR3 |= PWR_CR3_APC;
// Disable RTC alarm interrupt
NVIC_DisableIRQ(RTC_Alarm_IRQn);
NVIC_ClearPendingIRQ(RTC_Alarm_IRQn);
// Disable radio interrupt
NVIC_DisableIRQ(SUBGHZ_Radio_IRQn);
NVIC_ClearPendingIRQ(SUBGHZ_Radio_IRQn);
// Disable ADC interrupt
NVIC_DisableIRQ(ADC_IRQn);
NVIC_ClearPendingIRQ(ADC_IRQn);
// Disable TIM1 interrupt
NVIC_DisableIRQ(TIM1_CC_IRQn);
NVIC_ClearPendingIRQ(TIM1_CC_IRQn);
// Disable low power timer interrupts
NVIC_DisableIRQ(LPTIM1_IRQn);
NVIC_ClearPendingIRQ(LPTIM1_IRQn);
NVIC_DisableIRQ(LPTIM2_IRQn);
NVIC_ClearPendingIRQ(LPTIM2_IRQn);
NVIC_DisableIRQ(LPTIM3_IRQn);
NVIC_ClearPendingIRQ(LPTIM3_IRQn);
// Disable SysTick and interrupt
SysTick->CTRL &= ~(SysTick_CTRL_TICKINT_Msk | SysTick_CTRL_ENABLE_Msk);
NVIC_ClearPendingIRQ(SysTick_IRQn);
watchdog_kick();
// Check low power regulator is ready
while((PWR->SR2 & PWR_SR2_REGLPS) == 0);
// Enter standby
__WFI();
}
Please let me know if you would like any other pieces of code.
Thanks,
Rebecca
2022-06-01 5:45 PM
Hi all,
Turns out it was an issue between the seat and the steering wheel. I was looking at an updated schematic that used a pin for a different function, so my PU/PD resistors were set incorrectly. The MCU now enters and exits Standby mode correctly all the way down to 1.85V.
Thanks,
Rebecca
2022-06-05 5:24 AM
The chair and the keyboard in this case... ;)
PWR_SCR register and it's bits are write-only - read and OR operations are unnecessary.
There is no point in configuring the GPIOx and NVIC registers before going into standby or shutdown modes because those will be reset immediately anyway and will not have an impact in those modes. Indeed, if you need pull-up/down to be active in those modes, you must use PWR_PUCRx/PWR_PDCRx registers and PWR_CR3_APC bit.