2024-06-26 12:17 AM - last edited on 2024-06-26 1:52 AM by STTwo-32
hello everyone
i try to make same ping pong dual core example but my project not working can you help me to found the problem
"there is not fault in build and i can run the project but it not working"
i did not understan where is the problem
2024-06-26 1:52 AM
Hello @Humem_MHA
I suggest you compare your configuration to the configuration of this example and try to find the difference and why your code is not running.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-26 2:39 AM
I already configured it based on the example step by step, but I did not succeed in getting it to work, by the way when i make debug and try to run it Line by line some times it is working But this is not a solution
I guess there is problem with connection between cores or with clock , is it possible
2024-08-07 6:26 AM
What I suggest you is to try to update your Firmware and IDE to the last version. It may be an issue related to the Cube Firmware or tool.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.