STM32WL55 no rf
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-20 8:55 AM
Good day
I am using the STM32WL55 chip for a project. I did preliminary tests using the NUCLEO-WL55JC2 Development board.
I created a custom PCB following the design of the Development board.
When I program the custom board with the same firmware that works on the development kit I do not get any output on either the RFO_HP pin or the RFO_LP pin.
On the Custom board I have a crystal and not a TXCO. Can that configuration have a impact?
On the Custom board:
VDDRF = 3.3V, VDDPA = 3.3V ( I need the high power output)
VLXSMPS = 1.5V,
Is there someone that can suggest checks to do to find the fault?
Solved! Go to Solution.
- Labels:
-
STM32WL series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 8:55 AM
If you're using a crystal rather than a TCXO, you need to adjust the BSP_RADIO_IsTCXO function in stm32wlxx_nucleo_radio.c.
Also, for a crystal, radio_driver.c (SUBGRF_Init) loads the HSE trim capacitors with XTAL_DEFAULT_CAP_VALUE; if you haven't changed this, it will be 0x20. I've forgotten what the units are, but it turns out that this is very large -- enough to throw the oscillator timing off. We had designed-in external capacitors, so we used 0x00 instead. You may want something larger (0x08, maybe?). You can monitor the HSE32 via the MCO (PA8).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 8:55 AM
If you're using a crystal rather than a TCXO, you need to adjust the BSP_RADIO_IsTCXO function in stm32wlxx_nucleo_radio.c.
Also, for a crystal, radio_driver.c (SUBGRF_Init) loads the HSE trim capacitors with XTAL_DEFAULT_CAP_VALUE; if you haven't changed this, it will be 0x20. I've forgotten what the units are, but it turns out that this is very large -- enough to throw the oscillator timing off. We had designed-in external capacitors, so we used 0x00 instead. You may want something larger (0x08, maybe?). You can monitor the HSE32 via the MCO (PA8).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 9:36 AM
Good day
Thank you for the response.
I have decided to use the TCXO as it will give me much better reliability out in the field with temperature changes