cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL33KB 2.4GHz frequency band support

leahjoseph
Associate II

The datasheet of STM32WL33KB states that the frequency bands 159-185 MHz, 413-479 MHz, 826-958 MHz are supported.

image.png

However, the website mentions that "For greater flexibility, it supports wide frequency bands from 100 MHz – 2.4 GHz".

leahjoseph_1-1718883117832.png

Can I get some clarification as to whether 2.4 GHz is supported or not?

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @leahjoseph and welcome to the ST Community 😊

The 2.4GHz is supported only for on the Wake-up radio receiver and not for the Ultra-low power Sub-1GHz RX/TX transceiver. The STM32WL33 include two separated Radio modules:

STTwo32_0-1718900393634.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @leahjoseph and welcome to the ST Community 😊

The 2.4GHz is supported only for on the Wake-up radio receiver and not for the Ultra-low power Sub-1GHz RX/TX transceiver. The STM32WL33 include two separated Radio modules:

STTwo32_0-1718900393634.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.