2023-11-07 06:18 AM
Hi all,
I have three STM32WL55 boards and I am following the STM32WL_WS Workshop tutorial. I can programmed one of the boards using SubGHz_Phy_Base_Station.bin and build the sensor SubGHz_Phy_PingPong project for the other two boards using the following \Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\P2P_Sensor.
Both Sensor board works fine and I can edit both the c code header files in the project and program them. However if I edit the SubGHz_Phy_PingPong.ioc file then the project stops to build.
Has any one else experience this issue. Many thanks in advance.
Regards
Ola
Solved! Go to Solution.
2023-11-14 11:02 PM
Hi STTwo-32,
The problem has now been resolved. The problem was that when the any changes was made to the SubGHz_Phy_PingPong.ioc configuration file. The configuration wizard tools deletes most of the example code and leaves just a template code.
Regards
Ola
2023-11-13 01:49 AM
Hello @ola and welcome to the ST Community 😊.
Can you provide more information about the changes you have made on the SubGHz_Phy_PingPong.ioc so we can locate the problem better.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-14 11:02 PM
Hi STTwo-32,
The problem has now been resolved. The problem was that when the any changes was made to the SubGHz_Phy_PingPong.ioc configuration file. The configuration wizard tools deletes most of the example code and leaves just a template code.
Regards
Ola
2023-12-06 04:43 AM - edited 2023-12-06 05:58 AM
Moved to here
2023-12-06 04:59 AM
Hello @ola
Can you create a new topic and give a good description to your problem. This will give it more visibility and you can easily find an answer that may help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-06 05:18 AM
STTwo-32
I am happy to create a new topic but I am not sure what you mean by give a good description to your problem. As I just gave a good description of the problem with images.
Regards
Ola