Skip to main content
Phoenix
Associate
April 5, 2022
Solved

STM32WL CubeIDE "Could not verify ST device! Abort connection on core CM0+, CM4 working fine

  • April 5, 2022
  • 2 replies
  • 10948 views

During debugging of a dual core application everything works fine for the CM4 core debug config and afterwards starting the program. As soon as I try to add the debug config for CM0+ the following error occurs:

0693W00000Lww7tQAB.png

 
STMicroelectronics ST-LINK GDB server. Version 6.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61235
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 
 
Error in initializing ST-LINK device.
Reason: ST-LINK: Could not verify ST device! Abort connection.

I can reproduce the error using Nucleo-WL55JC1 with example dual core projects, so it is at least not my code. Tried onboard ST-link v3 and external STLINK V3SET.

I verified my config following this tutorial.

CubeMonitor and CubeProgrammer can connect without any issues.

This topic has been closed for replies.
Best answer by LaurentL

Hello,

This issue is confirmed, see answer on this post :

https://community.st.com/s/question/0D53W00001PxJDeSAN/stm32wl55-dual-core-debug-error-18-when-debugging-cm0

Rgds,

Laurent

2 replies

LaurentL
LaurentLBest answer
ST Employee
April 5, 2022
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Phoenix
PhoenixAuthor
Associate
April 5, 2022

Merci Laurent!

My searches didn't return this... I think I need to work on my Google-Fu ;)