cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WBA52 LSE as GPIO Issue

rajdeep_01
Associate III

Hi,

Requirement: Use LSE pins: PC14/PC15 as GPIO Output.
MCU: STM32WBA52CGU6
Issue: Output voltage not sustain at 3.3V but getting 3.152V (GPIO connected circuit consumes 300uA only).

- For clean firmware, generated firmware based on IOC, configured only these two pins as output, push-pull, High state.
- Attached related IOC-file, debug-SFR-states-screenshot and generated-project files.

I thinks that this is STM MCU level limitation and STM-Team must provide errata for same with workaround-status.

Please guide me in case anyone have known workaround.

Thanks

 

4 REPLIES 4
Peter BENSCH
ST Employee

Please check the current flowing from the GPIO and the voltage at VCC again. The output characteristics in the data sheet, table 70, result in some 50...65mohms internal Rdson, so that with your 0.3mA about 3.285V of the (hopefully) 3.3V should be measurable.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

What board is this on?

Please see the Posting Tips:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

Does the datasheet specify any restrictions on these pins when used as GPIO ?

Do other GPIOs reach 3.3V ?

rajdeep_01
Associate III

1. Part Number: STM32WBA52CGU6: (Checked in both Nucleo-WBA52CG & Custom-Board.)
2. Environment: SDK: V1.4.1, CMSIS: V5.9.0, STM32WBAxx CMSIS: V1.4.0, STM32CubeIDE V1.15.1 (GCC12).

@Peter BENSCH 

- Thanks for quick reply,
- Double checked that upon make GPIO left unconnected, then properly getting 3.3V but upon with minor resistance connected with only 300uA consumption, voltage down to 3.152V.
- Can you please share datasheet, because I have go through Datasheet, Reference-Manual & Errata but not able to find relevant information.
- Note that this case happens with only LSE GPIOs not with other GPIOs.

@Andrew Neil 
- Thanks for guide, I will try to cover all relevant information.
- No restriction mentioned on these LSE Pins for make work as GPIO, even informed that we can use those pins as GPIO.

Thanks.

rajdeep_01
Associate III

@Peter BENSCH 

Can you initiate process to mark LSE pins as GPIO issues in next errata release?

Thanks.