2024-11-13 12:16 PM
The product page shows that the STM32WBA50KG supports I2S for a serial audio interface. I want to connect a Class-D Amp and cannot find any reference to I2S or SAI in the data sheet or programmers reference manual. Does the processor support I2S?
Solved! Go to Solution.
2024-11-13 8:19 PM
Hello @JimRVLock
As you can see on the top of the page 1646 of the RM0493 Rev 5, the SAI is Available only on STM32WBA54/55xx devices. So, the STM32WBA50KG does not support the SAI/I2S.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-13 7:34 PM
Yes, the STM32WBA50KG includes various communication peripherals, including I2S functionality. This allows it to connect with audio devices such as Class D amplifiers.
2024-11-13 8:19 PM
Hello @JimRVLock
As you can see on the top of the page 1646 of the RM0493 Rev 5, the SAI is Available only on STM32WBA54/55xx devices. So, the STM32WBA50KG does not support the SAI/I2S.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-14 9:11 AM
Understood and I upgraded to the STMWBA54.
Just to be clear, the data in the product selector is wrong and should be corrected at some point, but it's not a problem at this point {see below screen shot}.
Thank you for the information and quick response to my question.