The sensor can be used in a vertical orientation. You need to adjust the data in your software to correct the magnetic field so that the sensor output is consistent with the actual direction.
This is quite a technical task. The user manual for the STM32Cube PDM2PCM software library might be useful for you. The documentation explains how to configure the library, set interface parameters, and how to convert PDM signals into PCM audio strea...
Make sure your Proteus software supports USB emulation. You need to install the appropriate USB drivers. You can find the “Virtual USB” option in the Proteus installation directory under the Start menu. Click on it and select “Install USB Drivers” to...
Yes, the STM32WBA50KG includes various communication peripherals, including I2S functionality. This allows it to connect with audio devices such as Class D amplifiers.