2020-11-19 8:27 AM
Hi.
In SDK I foud interesting source files: ble_events.h, ble_events.c, in wich we have 3 structures defined as hci_event_table_t.
Also in ble_legacy.h we have a defines to that structures.
Every strucrure have event code and callback and callback calls a process function which is a __WEAK.
But any examples dont use that feature.
Questions:
1. Can I use these files or are they temporary and after a while they can change dramatically or disappear?
2. Many event in that files not declared of those that are in "AN5270" (STM32WB Bluetooth® Low Energy (BLE) wireless interface). Why?
Solved! Go to Solution.
2020-11-25 10:20 AM
Hello,
1/ The ble_events. and ble_events.h will be kept in all deliveries and will be maintained.
Our examples are based on the other model which is more suitable for a generic scalable framework.
For a dedicated application where the number of services and characteristics is limited and well known in advance, then the event mechanism would be a nice alternative as it is more friendly to decode the received packet.
2/ If you spotted any mismatch between the AN5270 abd the ble_events.c/h files, this is not expected. I will report this to the dedicated team.
Do you have any mismatch example to provide ?
Regards.
2020-11-25 2:10 AM
?
2020-11-25 10:20 AM
Hello,
1/ The ble_events. and ble_events.h will be kept in all deliveries and will be maintained.
Our examples are based on the other model which is more suitable for a generic scalable framework.
For a dedicated application where the number of services and characteristics is limited and well known in advance, then the event mechanism would be a nice alternative as it is more friendly to decode the received packet.
2/ If you spotted any mismatch between the AN5270 abd the ble_events.c/h files, this is not expected. I will report this to the dedicated team.
Do you have any mismatch example to provide ?
Regards.
2020-11-25 10:28 AM
Christophe, thanks for nice answers.
About second question: I prepare many examples and put them in this topic.
Thanks.