2021-10-12 8:20 PM
I was trying to flash my STM32WB Nucleo board with the latest (v1.2.0) FUS image using the CubeProgrammer. However, it fails with the following error.
14:15:16 : Old Firmware delete ...
14:15:16 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
14:15:16 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
14:15:16 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
14:15:16 : Warning: Option Bytes are unchanged, Data won't be downloaded
14:15:16 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
14:15:16 : Memory Programming ...
14:15:16 : Opening and parsing file: 0x495_FUS_Operator.bin
14:15:16 : File : 0x495_FUS_Operator.bin
14:15:16 : Size : 8 KBytes
14:15:16 : Address : 0x08000000
14:15:16 : Erasing memory corresponding to segment 0:
14:15:16 : Erasing internal memory sectors [0 1]
14:15:16 : Download in Progress:
14:15:17 : File download complete
14:15:17 : Time elapsed during download operation: 00:00:00.267
14:15:17 : Application is running, Please Hold on...
14:15:24 : Reconnecting...
14:15:24 : Reconnected !
14:15:24 : Error: FUS_STATE_ERR_UNKNOWN
I tried "Start FUS" and "Read FUS infos" and got this:
It indicates that the FUS Version is v0.0.0.0, which looks quite weird! Besides, the option byte reading of the MCU is:
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF3736324D5043233624
ST-LINK FW : V2J38M27
Board : P-NUCLEO-WB55
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xd5
Debug in Low Power mode enabled
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x58004020
Size : 96 Bytes
██████████████████████████████████████████████████ 100%
Bank : 0x01
Address : 0x58004080
Size : 8 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
User Configuration:
nBOOT0 : 0x1 (nBOOT0=1 Boot from main Flash)
nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
nSWBOOT0 : 0x0 (BOOT0 taken from the option bit nBOOT0)
SRAM2RST : 0x0 (SRAM2 erased when a system reset occurs)
SRAM2PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDGSW : 0x1 (Software window watchdog)
IWGDSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDGSW : 0x1 (Software independent watchdog)
IPCCDBA : 0x0 (0x0)
Security Configuration Option bytes - 1:
ESE : 0x1 (Security enabled)
PCROP Protection:
PCROP1A_STRT : 0x1FE (0x80FF000)
PCROP1A_END : 0x0 (0x8000800)
PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
PCROP1B_STRT : 0x1FE (0x80FF000)
PCROP1B_END : 0x0 (0x8000800)
Write Protection:
WRP1A_STRT : 0xFF (0x80FF000)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x80FF000)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1
Security Configuration Option bytes - 2:
SFSA : 0xF6 (0x80F6000)
FSD : 0x0 (System and Flash secure)
DDS : 0x1 (CPU2 debug access disabled)
C2OPT : 0x1 (SBRV will address Flash)
NBRSD : 0x0 (SRAM2b is secure)
SNBRSA : 0x10 (0x2003C000)
BRSD : 0x1 (SRAM2a is non-secure)
SBRSA : 0x0 (0x20030000)
SBRV : 0x3D800 (0x20000000)
Could someone please kindly advise why I am getting this error ((FUS_STATE_ERR_UNKNOWN) and how I can solve this issue? Thanks in advance!
2021-10-12 10:24 PM
Could anyone help with this please? @Remi QUINTIN @Imen DAHMEN
2021-10-13 12:59 AM
According to the SFSA value, you still have the original FUS on your board.
Assuming you are using the latest WB FV v1.12, you must use the stm32wb5x_FUS_fw_for_fus_0_5_3. bin file to update the FUS.
I see you are using CubeProgrammer v2.8 and this is OK. Once you 'll manage to upgrade the FUS, you should be able to see the FUS version even when using the SWD port for the programming.
2021-10-13 3:41 PM
Thank you so much for your advice. However, I have tried programming stm32wb5x_FUS_fw_for_fus_0_5_3. bin but still failed with the same error:
PS C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin> .\STM32_Programmer_CLI.exe -c port=swd -fwupgrade C:\Users\myuser\STM32Cube\Repository\STM32Cube_FW_WB_V1.12.1\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_FUS_fw_for_fus_0_5_3.bin 0x080EC000
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF3736324D5043233624
ST-LINK FW : V2J38M27
Board : P-NUCLEO-WB55
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xd5
Debug in Low Power mode enabled
Old wireless stack delete ...
Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
Warning: Option Byte: nboot0, value: 0x1, was not modified.
Warning: Option Byte: nboot1, value: 0x1, was not modified.
Warning: Option Bytes are unchanged, Data won't be downloaded
Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
Memory Programming ...
Opening and parsing file: 0x495_FUS_Operator.bin
File : 0x495_FUS_Operator.bin
Size : 8 KBytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:00.311
Application is running, Please Hold on...
Reconnecting...
Reconnected !
Error: FUS_STATE_ERR_UNKNOWN
Error:
Old Firmware delete failed
Could you advise? Does it have something to do with the current "v0.0.0.0" FUS version? Thanks!
2021-10-14 12:29 AM
FUS_STATE_ERR_UNKNOWN means the FUS is not activated.
Could you tell me the value of the SBSFA and SBRV option bytes?
Try also press the "Start FUS" button and then read the FUS version.
2021-10-14 2:49 AM
The value of SBRV is 0x3D800 and as for the other option byte, SBRSA is 0x0, SNBRSA is 0x01, and SFSA is 0xF6. I also tried press "Start FUS" button and read the FUS version. The FUS version is "v0.0.0.0".
2021-10-14 5:02 AM
I really do not see any reason why the FUS version is not detected. The option byte values are OK.
Last trials:
2021-12-25 12:39 PM
Hi!)
Has the issue been resolved?
I have a similar problem. Previously, I successfully used WB55CGU6 (rev. Y) in my device, now I'm trying WB55CEU6 (rev. Y) (bought in June 2021 on Arrow.com ).
1. I tried to run on 5 boards in USB DFU mode - to no avail. I rechecked the OB combinations several times, physically pin BOOT0 to pull up to Vdd. The USB circuits actually work - I checked using a separate USB Mass Storage Device firmware.
2. When trying to work with FUS via SWD (of course at the changed addresses for CE), I get FUS_STATE_ERR_UNKNOWN errors.
3. Reading RAM at 0x20030890 gives all zeros.
Could these be "special" chips with damaged FUS?)
Help me) Thanks!
2022-01-14 8:50 AM
Before going any further , are you able to know the FW version of the FUS installed on your new boards?
Then Which FUS file do you want to program? Which WB FW version are you using?
a )Using the USB_USER port in DFU mode, be sure to set the PH3/BOOT0 pin to high and set the nSWBOOT0 option byte to 1 and nBOOT1 option byte to 1. NBOOT0 option byte is not applicable as the Value is set by the external BOOT0 pin. If those options bytes are not set properly, you need to revert to the SWD port to configure them.
Your new board is now having only 512KB flash memory. What is the FW stack to program? Did you check its size?
b) Now using SWD port, it looks like you are able to connect your board. In that case can you check and the FUS version?
2022-01-14 10:15 AM
1. An attempt to read the status and version of FUS via SWD ends with the error FUS_STATE_ERR_UNKNOWN
At the same time, the data in the first flash sectors changes from 0xFF to some data.
2.I use the FW_WB V1.10.1 version
FUS version: first stm32wb5x_FUS_fw_1_0_2.bin, after - stm32wb5x_FUS_fw.bin from FW_WB V1.10.1. addr: 0x0807A000.
3.I tried USB DFU again - it doesn't work! Under the same conditions on WB55CG - everything is OK
4. I use BLUE_STACK_FULL, ~162kB
Log from CubeProgrammer when trying to read FUS infos:
21:13:37 : Reconnected !
21:13:37 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
21:13:37 : Memory Programming ...
21:13:37 : Opening and parsing file: 0x495_FUS_Operator.bin
21:13:37 : File : 0x495_FUS_Operator.bin
21:13:37 : Size : 8 KBytes
21:13:37 : Address : 0x08000000
21:13:37 : Erasing memory corresponding to segment 0:
21:13:37 : Erasing internal memory sectors [0 1]
21:13:37 : Download in Progress:
21:13:37 : File download complete
21:13:37 : Time elapsed during download operation: 00:00:00.370
21:13:37 : Application is running, Please Hold on...
21:13:37 : Reconnecting...
21:13:37 : Reconnected !
21:13:37 : Error: FUS_STATE_ERR_UNKNOWN
21:13:37 : the Fus getState command Failed
21:13:37 : Read FUS state Operation Failure! Please, try again