cancel
Showing results for 
Search instead for 
Did you mean: 

DMA + ADC doesn't work

Stecklo
Senior

CubeIDE 1.1.0

STM32Cube_FW_WB_V1.3.0

Trying to make DMA transfer ADC results.

I'm putting code in main() after MX_..._Init() and before while(1) {}

HAL_ADC_Start_IT(&hadc1); works fine

HAL_DMA_Start_IT(&hdma_memtomem_dma1_channel2, (uint32_t) src, (uint32_t) dest, 40); works fine too

but

HAL_ADC_Start_DMA(&hadc1, dest, 10) doesn't work as it should

ADC is activated and keeps throwing Overrun_Error

But DMA doesn't transfer anything

static void MX_ADC1_Init(void)
{
 
  /* USER CODE BEGIN ADC1_Init 0 */
 
  /* USER CODE END ADC1_Init 0 */
 
  ADC_ChannelConfTypeDef sConfig = {0};
 
  /* USER CODE BEGIN ADC1_Init 1 */
 
  /* USER CODE END ADC1_Init 1 */
  /** Common config 
  */
  hadc1.Instance = ADC1;
  hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV8;
  hadc1.Init.Resolution = ADC_RESOLUTION_12B;
  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
  hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc1.Init.LowPowerAutoWait = DISABLE;
  hadc1.Init.ContinuousConvMode = ENABLE;
  hadc1.Init.NbrOfConversion = 1;
  hadc1.Init.DiscontinuousConvMode = DISABLE;
  hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
  hadc1.Init.DMAContinuousRequests = ENABLE;
  hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
  hadc1.Init.OversamplingMode = ENABLE;
  hadc1.Init.Oversampling.Ratio = ADC_OVERSAMPLING_RATIO_16;
  hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_NONE;
  hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
  hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_CONTINUED_MODE;
  if (HAL_ADC_Init(&hadc1) != HAL_OK)
  {
    Error_Handler();
  }
  /** Configure Regular Channel 
  */
  sConfig.Channel = ADC_CHANNEL_5;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
  sConfig.SingleDiff = ADC_DIFFERENTIAL_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN ADC1_Init 2 */
 
  /* USER CODE END ADC1_Init 2 */
 
}
static void MX_DMA_Init(void) 
{
 
  /* DMA controller clock enable */
  __HAL_RCC_DMAMUX1_CLK_ENABLE();
  __HAL_RCC_DMA1_CLK_ENABLE();
 
  /* Configure DMA request hdma_memtomem_dma1_channel2 on DMA1_Channel2 */
  hdma_memtomem_dma1_channel2.Instance = DMA1_Channel2;
  hdma_memtomem_dma1_channel2.Init.Request = DMA_REQUEST_MEM2MEM;
  hdma_memtomem_dma1_channel2.Init.Direction = DMA_MEMORY_TO_MEMORY;
  hdma_memtomem_dma1_channel2.Init.PeriphInc = DMA_PINC_ENABLE;
  hdma_memtomem_dma1_channel2.Init.MemInc = DMA_MINC_ENABLE;
  hdma_memtomem_dma1_channel2.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
  hdma_memtomem_dma1_channel2.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
  hdma_memtomem_dma1_channel2.Init.Mode = DMA_NORMAL;
  hdma_memtomem_dma1_channel2.Init.Priority = DMA_PRIORITY_LOW;
  if (HAL_DMA_Init(&hdma_memtomem_dma1_channel2) != HAL_OK)
  {
    Error_Handler( );
  }
 
  /* DMA interrupt init */
  /* DMA1_Channel1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 15, 0);
  HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 
}
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  if(hadc->Instance==ADC1)
  {
  /* USER CODE BEGIN ADC1_MspInit 0 */
 
  /* USER CODE END ADC1_MspInit 0 */
    /* Peripheral clock enable */
    __HAL_RCC_ADC_CLK_ENABLE();
  
    __HAL_RCC_GPIOA_CLK_ENABLE();
    /**ADC1 GPIO Configuration    
    PA0     ------> ADC1_IN5
    PA1     ------> ADC1_IN6 
    */
    GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
    /* ADC1 DMA Init */
    /* ADC1 Init */
    hdma_adc1.Instance = DMA1_Channel1;
    hdma_adc1.Init.Request = DMA_REQUEST_ADC1;
    hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
    hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
    hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
    hdma_adc1.Init.Mode = DMA_NORMAL;
    hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;
    if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
    {
      Error_Handler();
    }
 
    __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
 
  /* USER CODE BEGIN ADC1_MspInit 1 */
 
  /* USER CODE END ADC1_MspInit 1 */
  }
 
}

I've tried this confuguration on PNUCLEO-WB55 Dongle in far more complex code and it worked. Now I'm using custom board and just main() body. But I think the board should not matter as DMA is totally internal thing

1 ACCEPTED SOLUTION

Accepted Solutions
Stecklo
Senior

The answer is to put

MX_DMA_Init();

before

MX_ADC1_Init();

As the first one calls

__HAL_RCC_DMAMUX1_CLK_ENABLE();

 __HAL_RCC_DMA1_CLK_ENABLE();

View solution in original post

25 REPLIES 25
Ozone
Principal

I don't know the WB55 device, and usually do not play with Cube code.

Have you checked the DMA (instance/channel) is correct ?

Stecklo
Senior

I'm away from my PC now. But the code above looks like it should work (it is all auto generated by CubeMX). Altough I can't see the explicit initialization of hadc->DMA_handle. But Ithink it is handled in __HAL_LINKDMA()

Read out and check the DMA and DMAMUX registers.

> hdma_memtomem_dma1_channel2.Init.Request = DMA_REQUEST_MEM2MEM;

> hdma_memtomem_dma1_channel2.Init.Direction = DMA_MEMORY_TO_MEMORY;

Most probably not.

JW

Stecklo
Senior

@Community member​ , you were right.

DMAMUX_CxCR is empty

This line does nothing. While operands are 5 and 255. The result should be 5, but CCR is 0.

HAL_StatusTypeDef HAL_DMA_Init(DMA_HandleTypeDef *hdma) 
{
    <...>
    hdma->DMAmuxChannel->CCR = (hdma->Init.Request & DMAMUX_CxCR_DMAREQ_ID);
    <...>
}

I havent located the reason so far, but this is a good clue.

Stecklo
Senior

The answer is to put

MX_DMA_Init();

before

MX_ADC1_Init();

As the first one calls

__HAL_RCC_DMAMUX1_CLK_ENABLE();

 __HAL_RCC_DMA1_CLK_ENABLE();

Stecklo
Senior

Is there any way to make CubeMX aka Device Configuration Tool to change the Init functions order? There is a corresponding view in Project Manager tab, but the order seems to be fixed.

Stecklo
Senior

Well, I've changed the order manually editing .ioc file with text editor. But the whole thing should be considered as a CubeMX bug

Amel NASRI
ST Employee

Hello,

Glad that you found the root cause of your issue.

I'll report this limitation to our STM32CubeMX team.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @Community member​ 

Thanks for the feedback,

It will be fixed on the next version of CubeMX.

Best regards,

Nesrine