2023-02-09 2:45 AM
After following these examples I am unable to put the device in STOP1/2 low power modes.
Can someone please help with implementing low-power modes
2023-02-10 2:00 AM
Hello @Community member
Could you precise what is exactly the issue? or errors u get?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-10 2:07 AM
Hi @Sarra.S
Thank You,
I followed examples to implement low power modes, if I try to put the device into STOP2 and STOP1 modes the power consumption should be around 2µA as per the datasheet in STOP2.
But it still consuming 10mA in both cases.
I believe it's not entering into low-power mode.
I followed some post also but no improvements
2023-02-10 2:45 AM
Hello again @Community member
I think you missing something in the configuration
Could you share your .ioc file and your main.c so I can check the problem
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-10 3:26 AM
2023-02-12 7:44 PM
Hi @Sarra.S ,
Is there anything I am missing in the configuration?
2023-03-02 1:46 AM
Hi @Sarra.S ,
Now I am able to put the device to sleep mode perfectly.
But when the button pressed device wakes up but Sequencer not working, even after calling SystemClock_Config(); HAL_ResumeTick(); Sequencer not working.
if I remove the sleep code Sequencer works fine.
please can you help me with this problem?
Thank You,
2023-03-02 3:05 AM
Hello @Community member
Here is a list of resources relating to use of the sequencer with the STM32WB55:
Building wireless applications with STM32WB Series microcontrollers
STM32WB Bluetooth® Low Energy (BLE) wireless interface
STM32WB – BLE SW Application Architecture
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-02 6:32 AM
Hi again @Sarra.S ,
Yes, I have followed the same steps from the post, I tried giving priority to my tasks from 15. still, I am facing the same issue. I am not understanding the root cause.
//===================My sleep code =======================
while (1)
{
/* USER CODE END WHILE */
MX_APPE_Process();
/* USER CODE BEGIN 3 */
if(Go_TO_SLEEP)
{
Go_TO_SLEEP = false;
HAL_GPIO_WritePin(MY_LED_GPIO_Port, MY_LED_Pin,1);
HAL_Delay(5000);
HAL_GPIO_WritePin(MY_LED_GPIO_Port, MY_LED_Pin,0);
GPIO_InitStructure.Pin = GPIO_PIN_All;
GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
GPIO_InitStructure.Pull = GPIO_NOPULL;
// HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
// HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOD, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOE, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);
// __HAL_RCC_GPIOA_CLK_DISABLE();
// __HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
__HAL_RCC_GPIOE_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
DBGMCU->CR = 0;
HAL_SuspendTick();
LL_C2_PWR_SetPowerMode(LL_PWR_MODE_STOP2);
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
}
}
========================================================
//===========Button ISR======================================
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
SystemClock_Config();
HAL_ResumeTick();
Current_Button = GPIO_Pin;
ISR_func();
UTIL_SEQ_SetTask(1 << CFG_TASK_ISR_CALLBACK, 15);
}
==========================================================
2023-06-23 3:06 AM
Hello @AM.12
We are using a custom board which has stm32wb55 as the MCU. Even I followed the example project and replicated the same on to my project. But the current consumption is around 300uA and unable to get around 3uA as per the datasheet. Were you able to solve the issue on your side? If yes, can you help me as well??
Thanks