cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 IrDA hardware setup

Tvan .15
Associate

after looking over all the documentation i could find (datasheet, reference manual, etc.), i could not clearly find how i am meant to connect IR LED(s) for IrDA communication with an STM32WB55. The image i attached is a screenshot from the reference manual, which implies that there may be IrDA_OUT and _IN pins (i'm interpreting this as being seperate from the TX and RX pins). Am i supposed to add some kind of intermediate IC for IrDA, or can the STM32WB55 actually output signals for driving/reading IR LEDs/photodiodes?

 

P.S. i'm aware of the existance of the IR_OUT pins, but that appears to be its own seperate thing. In the IR_OUT documentation they use only timers (TIM16 & TIM17), not the USART peripheral.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

IrDA has hardly been used for a long time, which is also noticeable in discontinued IrDA transceivers. However, since essentially everything except the TIA and optical components is included in the STM32 IrDA SIR ENDEC, it is possible to recreate IrDA with

  • an IR LED plus driver transistor and
  • an IR photodiode plus TIA.

As @MM..1​  said, RX and TX are switched to the IrDA function so that LED driver and TIA can be connected directly.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
MM..1
Chief III

Yes not clean , but i mean TX and RX is changed into IR after HAL IRDA init ...

Peter BENSCH
ST Employee

IrDA has hardly been used for a long time, which is also noticeable in discontinued IrDA transceivers. However, since essentially everything except the TIA and optical components is included in the STM32 IrDA SIR ENDEC, it is possible to recreate IrDA with

  • an IR LED plus driver transistor and
  • an IR photodiode plus TIA.

As @MM..1​  said, RX and TX are switched to the IrDA function so that LED driver and TIA can be connected directly.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

alright, thank you!