2022-05-10 08:58 AM
STM32WB55RGV6 connects ADS1299 by spi. And I choose spi2. There are three signas miso\ mosi and sck. SPI2 has two alternative: GPIO_AF3_SP2 and GPIO_AF5_SPI2.
① STM32CUBEMX automatically generated miso(GPIO_AF3_SP2), mosi and sck(GPIO_AF5_SPI2).Initialization is ok, but no data.
② All GPIO_AF3_SP2. Initialization is failed and application crash.
③ All GPIO_AF5_SP2. Successfully.
Although the result is good, I do not understand why
Solved! Go to Solution.
2022-05-10 09:31 AM
Which pins?
Look at the Alternate functions table in the datasheet to determine, which AF number to use for each pin.
For example:
JW
2022-05-10 09:31 AM
Which pins?
Look at the Alternate functions table in the datasheet to determine, which AF number to use for each pin.
For example:
JW
2022-05-10 09:45 AM
Thank you,I found the error,SCK(PD1), GPIO_AF5_SPI2.