2021-08-28 1:29 PM
From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says:
"This application is used to demonstrate the OpenThread Border router feature using an STM32WB device.
To play with the demo, you need a Raspberry Pi 3B (RPi) to perform the link with Wi-Fi/Ethernet networks
The full setup and the associated documentations can be requested to ST on demand".
Where can I find the full setup and associated documentation?
Thank you,
2021-08-31 7:31 AM
I need to check what documentation we could provide considering your case.
2021-10-15 1:13 AM
@Remi QUINTIN Is there any chance to also receive this documentation? I am looking for option to use STM32WB as a border router with raspberry by example. I checked Thread_RCP project but general documentation doesn't provide much information.
2021-11-16 2:15 AM
Hi,
I'm also interrested to know how to use the stm32wb55 with the openthread RCP stack/firmware.
@Remi QUINTIN Could you tell me where to find the associated documentation ?
Also, do you have plan to support the spinnel protocol (over uart/usb or spi) to communicate with the stm32wb55 as a ncp device ?
Thanks for your help.
2021-11-22 2:58 PM
Hi, is there an update on the documentation for the RCP firmware for the STM32WB?
2021-11-23 12:21 PM
Hi,
@Remi QUINTIN Could you tell me where to find the associated documentation? I will try STM32WB as a border router with RPI3.
2022-01-13 5:22 AM
2022-01-13 6:59 AM
Thank you!
2022-11-11 6:10 PM
Thanks for this documentation.
Where can I download this "OTBR_CLI_RPi_1.0.img" to flash?
2022-11-16 5:48 PM
I want to build this demo too.
Please attach OTBR_CLI_RPi_1.0.img here.
Or. . . Please give me some information.
Can I create an RPi RCP image with the following steps?
https://openthread.io/guides/border-router/raspberry-pi
Regards