2018-05-11 1:33 AM
Hi
I am using B-L072Z-LRWAN STM32 Eval board for configuring sensor.The sensor gives PWM as output.To measure the width I am using GPIOA 5 (PA5) pin as Timer input.I am using the following code for Timer configuration:
&sharpdefine TIMx TIM2
&sharpdefine TIMx_CLK_ENABLE() __HAL_RCC_TIM2_CLK_ENABLE()/* Definition for TIMx Pins */
&sharpdefine TIMx_CHANNEL_GPIO_PORT() __HAL_RCC_GPIOA_CLK_ENABLE()&sharpdefine GPIO_PORT GPIOA&sharpdefine GPIO_PIN_CHANNEL2 GPIO_PIN_5&sharpdefine GPIO_AF_TIMx GPIO_AF5_TIM2/* Definition for TIMx's NVIC */
&sharpdefine TIMx_IRQn TIM2_IRQn&sharpdefine TIMx_IRQHandler TIM2_IRQHandler/* Timer handler declaration */
TIM_HandleTypeDef TimHandle;/* Timer Input Capture Configuration Structure declaration */
TIM_IC_InitTypeDef sConfig;/* Slave configuration structure */
TIM_SlaveConfigTypeDef sSlaveConfig;/* Captured Value */
uint32_t uwIC2Value = 0;uint32_t uwIC2Value_f = 0;/* Duty Cycle Value */uint32_t uwDutyCycle = 0;/* Frequency Value */uint32_t uwFrequency = 0;void HAL_TIM_IC_MspInit(TIM_HandleTypeDef *htim) {PRINTF('IOINIT\n');GPIO_InitTypeDef GPIO_InitStruct;/*♯♯-1- Enable peripherals and GPIO Clocks ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* TIMx Peripheral clock enable */TIMx_CLK_ENABLE();/* Enable GPIO channels Clock */
TIMx_CHANNEL_GPIO_PORT();/* Configure (TIMx_Channel) in Alternate function, push-pull and 100MHz speed */
GPIO_InitStruct.Pin = GPIO_PIN_CHANNEL2@♯GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;GPIO_InitStruct.Pull = GPIO_PULLUP;GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;GPIO_InitStruct.Alternate = GPIO_AF_TIMx;HAL_GPIO_Init(GPIO_PORT, &GPIO_InitStruct);/*♯♯-2- Configure the NVIC for TIMx ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* Set the TIMx priority *///PRINTF('%d\n\r', TIMx_IRQn);HAL_NVIC_SetPriority(TIMx_IRQn, 0, 1);/* Enable the TIMx global Interrupt */
HAL_NVIC_EnableIRQ(TIMx_IRQn);}void Pwm_sensor_init(void)
{/*♯♯-1- Configure the TIM peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* Set TIMx instance */
TimHandle.Instance = TIMx;/* Initialize TIMx peripheral as follow:
+ Period = 0xFFFF+ Prescaler = 0+ ClockDivision = 0+ Counter direction = Up*/TimHandle.Init.Period = 0xFFFF;TimHandle.Init.Prescaler = 0;TimHandle.Init.ClockDivision = 0;TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP; if(HAL_TIM_IC_Init(&TimHandle) != HAL_OK){/* Initialization Error */PRINTF('ERROR\n\r');}/*♯♯-2- Configure the Input Capture channels ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* Common configuration */sConfig.ICPrescaler = TIM_ICPSC_DIV1;sConfig.ICFilter = 0;/* Configure the Input Capture of channel 1 */
sConfig.ICPolarity = TIM_ICPOLARITY_RISING;sConfig.ICSelection = TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&TimHandle, &sConfig, TIM_CHANNEL_1) != HAL_OK){/* Configuration Error */PRINTF('ERROR\n\r');}/* Configure the Input Capture of channel 2 */
sConfig.ICPolarity = TIM_ICPOLARITY_FALLING;sConfig.ICSelection = TIM_ICSELECTION_INDIRECTTI;if(HAL_TIM_IC_ConfigChannel(&TimHandle, &sConfig, TIM_CHANNEL_2) != HAL_OK){/* Configuration Error */PRINTF('ERROR\n\r');}/*♯♯-3- Configure the slave mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*//* Select the slave Mode: Reset Mode */sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET;sSlaveConfig.InputTrigger = TIM_TS_TI1FP1;sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_NONINVERTED;sSlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;sSlaveConfig.TriggerFilter = 0;if(HAL_TIM_SlaveConfigSynchronization(&TimHandle, &sSlaveConfig) != HAL_OK){/* Configuration Error */PRINTF('ERROR\n\r');} /*♯♯-4- Start the Input Capture in interrupt mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/if(HAL_TIM_IC_Start_IT(&TimHandle, TIM_CHANNEL_1) != HAL_OK){/* Starting Error */PRINTF('ERROR\n\r');} /*♯♯-5- Start the Input Capture in interrupt mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*///if(HAL_TIM_IC_Start(&TimHandle, TIM_CHANNEL_2) != HAL_OK)//{/* Starting Error */// PRINTF('ERROR\n\r');// }//PRINTF('%d\n\r',__HAL_TIM_GET_FLAG(&TimHandle,TIM_FLAG_CC1));
//PRINTF('%d\n\r',__HAL_TIM_GET_FLAG(&TimHandle,TIM_FLAG_CC2));// PRINTF('Init Done\n\r');}/**
* @brief Input Capture callback in non blocking mode * @param htim : TIM IC handle* @retval None*/void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){PRINTF('Interrupt\n\r');/*♯♯-5- Start the Input Capture in interrupt mode ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/if(HAL_TIM_IC_Start(&TimHandle, TIM_CHANNEL_2) != HAL_OK){/* Starting Error */PRINTF('ERROR\n\r');}if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1){/* Get the Input Capture value */uwIC2Value = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);if (uwIC2Value != 0)
{/* Duty cycle computation */uwDutyCycle = ((HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1)) * 100) / uwIC2Value;/* uwFrequency computation
TIM4 counter clock = (RCC_Clocks.HCLK_Frequency)/2 */ uwFrequency = (HAL_RCC_GetHCLKFreq())/2 / uwIC2Value;}
else{uwDutyCycle = 0;uwFrequency = 0;}// PRINTF('DUTY : %d\n\r', uwDutyCycle);// PRINTF('FREQUENCY : %d\n\r', uwFrequency);}I have added TIMx_IRQHandler in stm32l0xx_it.c and stm32l0xx_it.h files.
CC1IF flag is set in the Status Register of the timer but Interrupt Handler is not getting called.
Is there anything else that has to be configured?
#stm32l0-timer #b-l072z-lrwan1 #interrups2018-05-11 11:53 AM
I have added TIMx_IRQHandler in stm32l0xx_it.c and stm32l0xx_it.h files.
And where is the
#define TIMx_IRQHandler TIM2_IRQHandler
line? Is it in a common header included also in stm32l0xx_it.c? If not, then rename the handler in stm32l0xx_it.c explicitly to TIM2_IRQHandler(),
JW
2018-05-14 1:39 AM
Hi
Waclawek.Jan
,Thanks
After changing the name to TIM2_Handler I am getting interrupt.
How to calculate width using input capture?I used the following logic but seems to be getting wrong width value.
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{ if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) { HAL_TIM_IC_Start_IT(&TimHandle, TIM_CHANNEL_2);//Start the timer after rising edge to calculate widthuwIC2Value = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2);
}
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_2) { uwIC2Value_f = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2);//Capture value at falling edge and stop timer HAL_TIM_IC_Stop_IT(&TimHandle, TIM_CHANNEL_2); HAL_TIM_IC_Stop_IT(&TimHandle, TIM_CHANNEL_1); } PRINTF('%d\n\r', uwIC2Value_f - uwIC2Value);2018-05-14 4:19 AM
I don't know - I don't use Cube/HAL, sorry.
JW
2018-05-14 8:30 AM
Ok Thanks