cancel
Showing results for 
Search instead for 
Did you mean: 

Use of X-NUCLEO-LPM01A with STM32L072

Sujan Nag
Associate
Posted on May 22, 2018 at 12:32

Hello everyone, 

This is my first post here.

As part of my research with LoRaWAN, I am working on a custom built board having an STM32L072 module. One of the critical sections of my research involves calculating the energy consumption during transmission and reception. Hence I am looking for a method to power the board using 3.3v and log the voltage and current consumption.

As so I came across X-NUCLEO-LPM01A. According to its datasheet:

'It can be used to supply and measure the consumption of STM32 Nucleo-32, Nucleo-64 or Nucleo-144 boards, using Arduino connectors. Alternatively, it supplies and measures the consumption of any target connected by wires via the basic connector.'

My custom built board simply needs a VCC and a GND to operate. So I was wondering if

X-NUCLEO-LPM01A will suffice for this project. I was not able to find any video demonstrating the same. 

Please advice.

Thanks

Sujan.

#power-measurement #stm32l072 #lorawan #x-nucleo-lpm01a
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0