2025-01-23 8:12 PM - last edited on 2025-01-25 2:30 AM by Andrew Neil
Hello,
i try to program LSM100A ( STM32WLE5CC ) .
i can connect but can't program an elf file : error fail to erase memory, then cube programmer crashed.
thank you for support
logs :
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x000078ae2276d917, pid=43070, tid=0x000078ae31bff6c0
#
# JRE version: OpenJDK Runtime Environment (8.0_382-b06) (build 1.8.0_382-b06)
# Java VM: OpenJDK 64-Bit Server VM (25.382-b06 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libCubeProgrammer_API.so+0x16d917] checkDeviceConnection+0xa7
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again
#
# An error report file with more information is saved as:
# /home/dam/STM32CubeProgrammer/bin/hs_err_pid43070.log
#
# If you would like to submit a bug report, please visit:
# https://bell-sw.com/support
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
STM32CubeProgrammer/bin/STM32CubeProgrammer : ligne 5 : 43070 Abandon (core dumped) GDK_BACKEND=x11 "$DIR"/jre/bin/java -Djdk.gtk.version=2 -jar "$DIR/STM32CubeProgrammerLauncher" 2> /dev/null
Solved! Go to Solution.
2025-01-25 4:38 AM - edited 2025-01-25 4:39 AM
It semes that you are using a clone ST-LINK V2, so we can’t guarantee that it will work fine. Please ensure that you are using a genuine ST-LINK V2 to guarantee that it will work fine. More details are available in this article.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-25 2:10 AM
Hello @dam74
What is the ST-LINK that you are using and après you using the last cube programmer version V2.18.0. also, you can contact the înternal support of ours partner that works on this product.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-25 3:55 AM
I'm using V2.18.0.
Here's the STlink I'm using with STM32F103 also.
2025-01-25 4:38 AM - edited 2025-01-25 4:39 AM
It semes that you are using a clone ST-LINK V2, so we can’t guarantee that it will work fine. Please ensure that you are using a genuine ST-LINK V2 to guarantee that it will work fine. More details are available in this article.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-27 12:51 PM
thank you for your reply.
i test with a stlink v3 minie, it's all fine !