cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE project for BLE 5.4 PAwR feature on NUCLEO-WB09KE

makarchie
Associate

Hi everyone,

I’m a beginner with STM32 boards and I’m trying to understand and work with the BLE 5.4 PAwR feature. I have a NUCLEO-WB09KE board, and I’m using Windows 11 along with the STM32Cube_FW_WB0_V1.1.0 package. I have installed all the required tools: STM32CubeIDE, STM32CubeMX, and STM32CubeProgrammer.

I’m trying to replicate the example from this workshop video:
Workshop Video – BLE PAwR Example

I’ve also reviewed the README.md files in the following repositories:
1. STM32WB0-BLE-PAwR-ESL
2. STM32WB0x-Demo-Workshop

However, in the examples located at:
…/Projects/Applications/BLE_PAwR_Broadcaster

…/Projects/Applications/BLE_PAwR_Observer

I couldn’t find any folder for STM32CubeIDE (or a corresponding .ioc file). Only folders for IAR (EWARM) and Keil (MDK-ARM) are present, but I want to work with STM32CubeIDE.

Could someone please advise:

  • Is it possible to convert an EWARM / MDK-ARM project to STM32CubeIDE and generate a .ioc file?
  • What is the recommended step-by-step procedure to create a new STM32CubeIDE project from scratch (copying the source code) for BLE_PAwR_Broadcaster and BLE_PAwR_Observer?
  • Additionally, is it possible to modify the BLE_Beacon example (or use it as a reference) to create a project for STM32CubeIDE?

Any guidance or example would be greatly appreciated!

0 REPLIES 0