2024-07-08 03:38 AM - edited 2024-07-08 03:49 AM
My STM32 WBA55CG was working absolutely fine yesterday and today it seems that, my system refuses to find it. I have checked that i can see it from my device manager but when trying to flash it. It doesn't seem to do anything.
When i remove the JP2 jumper, it seems to turn on LD4. I have not removed the jumpers at all. They are as they came to me in the box.
I am able to see it on the STLink Upgrade utility which is in the cube ide.
Could it be because the ST-link chip is working fine but something is wrong with the microprocessor?
2024-07-08 05:45 AM
Hello @BadEngineer and welcome to the ST Community 😊.
If you remove the JP2, you will not be able to program or debug any code. If not, can you please try to upgrade the St-link firmware using CubeMX. Can you also ensure that you are using a data cable and not just a charging one.
Also, please ensure that the Jumpers are set as mentioned on the STM32WBA Nucleo-64 board (MB1863) - User manual
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-08 07:01 AM
@STTwo-32 Thank you for your reply.
I can confirm that i am using a micro usb cable that has the data lines (without the data lines it doesn't detect the unit at all).
I can confirm my JP2 and JP1 jumpers are on. I have attached some additional pictures to this.
I am using cube ide for this project, you can see through that, i am able to program up the stlink chip
When it comes to flashing it says no device found on target. i can confirm that my reset configuration is "Connect under reset"
2024-07-08 07:07 AM
Can you try to program it using Cube Programmer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-08 07:12 AM
@STTwo-32 Ty for your suggestion.
I have tried using stm32cube programmer but it can't seem to detect it at all (below is an image). I've tried UART, st-link and USB. None of them seem to detect it.
My device manager does detect it as shown from the image.
2024-07-08 08:21 AM
I think the MCU is broken in this case. I suggest you try using another Board or change the MCU.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-08 08:54 AM
2024-08-06 07:00 AM
Hello @BadEngineer
Could you please try to connect it to Cube Programmer throw ST-LINK and not UART mode (using a Data cable and not a charging one).
Best Regards.
STTow-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.