2024-11-12 4:43 PM - last edited on 2024-11-12 11:55 PM by STTwo-32
When will ST support Lora Basics Modem and, perhaps, Relay, FUOTA?
Thank you,
Dana
Solved! Go to Solution.
2024-11-12 11:54 PM - edited 2025-03-07 12:53 AM
Throw the STM32CUBEWL V1.3.0, ST is already implementing LoRa Basic Modem that will let you create an end-node application operating on SubGHZ frequencies. FUOTA it is also implemented on the Same SDK. You may refer to the AN5554. Finally, for the LoraWAN Relay, we Plan to integrate it on the future releases of the STM32CubeWL. But for now, you may need to do the implementation since is not yet supported on the current stack.
PS: I've created a new question since your original question is an old thread so I can give it more visibility.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-12 11:54 PM - edited 2025-03-07 12:53 AM
Throw the STM32CUBEWL V1.3.0, ST is already implementing LoRa Basic Modem that will let you create an end-node application operating on SubGHZ frequencies. FUOTA it is also implemented on the Same SDK. You may refer to the AN5554. Finally, for the LoraWAN Relay, we Plan to integrate it on the future releases of the STM32CubeWL. But for now, you may need to do the implementation since is not yet supported on the current stack.
PS: I've created a new question since your original question is an old thread so I can give it more visibility.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-13 6:28 PM
Thank you so much for the timely answer!
Looking at FW v1.3, it appears to retain the source structure of the LoRaMac reference stack; do I understand functionality has been merged into this from the LoRa Basics Modem stack? (rather than the LoRa Basics Modem stack being entirely adopted in v1.3)
Not complaining, just want to understand more depth. I truly appreciate the quality of FW v1.3 and have deployed 1k+ LoRaWAN nodes based on it.
Thanks,
Dana
2025-03-06 10:35 PM
Looking forward to LoRaWAN Relay support in STM32CubeWL.
Can you offer any sense of timing on STM32CubeWL releases, and when Relay might be added - weeks, months, before end 2025?
Thank you,
Brendon.