2021-01-13 02:22 AM
Just got two of the WL55JC1 boards today, and while working just fine transmitting data, the usb connectors are really bad. Can barely touch the usb without it disconnecting and resetting the board..
I will try and resolder the connector and see if this helps.
2021-01-13 02:48 AM
Are you charged with static electricity an discharge when you touch the connector?
2021-01-13 02:50 AM
Discarged. But it also happens when i move the cable around a bit, so most def a soldering/connectivity issue. Tried with multiple new cables as well.
2021-01-13 04:49 AM
Bad cables are also quite often.