2022-05-24 2:53 AM
Hi
i'm just sitting and messing with a few lora boards.
I find that nucleo-WL55JC1 has approx 10dbm RSSI better than seeed LoRa-E5, and that nucleo-WL55JC1 also transmits with a more powerful signal, what is your experience ??
with best regards
Solved! Go to Solution.
2024-01-25 10:00 AM
What do you mean exactly when you said the clock domain on one GPIO wasn't right? Which pin?
I see an issue in my application where the receiver appears to be desensed about 10 dB. I'm wondering if I have the same problem that you were seeing.
2024-01-25 10:40 AM
@DWalk.3 You're replying to a nearly two year old thread, and it doesn't seem that @spa23 has had any activity on the forum since then.
@DWalk.3 wrote:I'm wondering if I have the same problem that you were seeing.
The problem stated was with an RF switch control pin - so, if you have an RF switch, check that its control pins are really in the state they should be in...
2024-01-25 11:39 AM
I saw that after the fact. It looks like my RF pins are correct.