2024-01-16 06:02 AM
Greetings,
Can I replace NX3L1T3157GM analog switches on en.MB1389-WL55JC-highband-E02_Schematic with FSA5157L6X ?
Thanks in advance
Solved! Go to Solution.
2024-01-16 06:28 AM
Apart from the slightly higher capacitance values, which probably don't play a major role in this board as only DC is switched, the FSA usually shows even better values than the NX3, so in my opinion you should be able to use the FSA5157.
Hope that helps?
Good luck!
/Peter
2024-01-16 06:28 AM
Apart from the slightly higher capacitance values, which probably don't play a major role in this board as only DC is switched, the FSA usually shows even better values than the NX3, so in my opinion you should be able to use the FSA5157.
Hope that helps?
Good luck!
/Peter
2024-01-16 11:29 PM
Thank you Peter for your answer. Appreciate!