2022-01-14 1:30 AM
Hi i am developing a BLE-UART bridge with an STM32WB5M.
I am guetting around 1,85 KB/s data troughput, is this normal?
Did anyone pull this off with greater data troughput? (same uart thing or any streaming application)
Solved! Go to Solution.
2022-03-21 2:27 AM
I found out the data trougput depends a LOT of the BLE chipset of the android phone/device.
My phone didnt have BLE5.0 2M high speed support.
Newer i-phones and Samsung phones/tablets would be able to archieve this data trougputs.
2022-01-14 1:43 AM
Increasig baudrates:
2022-01-18 2:19 AM
When increasing the baud rate, you need to manage the flow control of the UART port. is it the case?
You can have a look at the BLE_DataThroughput project to see the maximum achievable throughput.
2022-01-18 2:47 AM
thanks @Remi QUINTIN
I had a couple of bugs going on regarding my DMA handling of the uart, i still need to get into that.
>>When increasing the baud rate, you need to manage the flow control of the UART port. is it the case?
I very didnt, thats maybe why my programm crashed.
>>You can have a look at the BLE_DataThroughput project to see the maximum achievable throughput.
Thanks!, just what i needed.(i find here people managing to get up to 90KBs data transfers with BLE_DataThroughput example, that would work for me)
I am about to drop the towel with BLE because i need a data troughput an order of magnitude higher than 2kB/s.
I seen in this ST OTA demo video they get around 180B/s speed (thats even worse)
2022-01-18 3:59 AM
i ran the BLE_DataThroughput example with PHY=2MBs
The terminal says im transmitting in between 170KB/s and 75KB/s.
Those are great news, but now i have more questions
Searching for what data is being accounted for:
inside dt_client_app.c:
static void DataThroughput_Calculation( void )
{
uint32_t MoyData;
if (Nbr_packet < 600)
{
Nbr_packet++;
TotalDataReceived += DataThroughputValue;
}
if (Nbr_packet == 600)
{
MoyData = TotalDataReceived / 600;
APP_DBG_MSG("Moy = %ld bytes/s \n",MoyData);
TotalDataReceived = 0;
Nbr_packet = 0;
}
APP_DBG_MSG("DT = %ld bytes/s lost = %ld \n",DataThroughputValue, packet_lost_local);
}
static void DataThroughputTimer( void )
{
DataThroughputValue = (uint32_t)(DataTransfered / TIMEUNIT);
packet_lost_local = (uint32_t)(packet_lost / TIMEUNIT);
DataTransfered = 0;
packet_lost = 0;
UTIL_SEQ_SetTask(1 << CFG_TASK_APP_DATA_THROUGHPUT_ID, CFG_SCH_PRIO_0);
return;
}
It looks indeed like its the real data troughput
DataTransfered += NotificationData.DataTransfered.Length;
2022-03-18 7:37 AM
Hello,
The data throughput is smaller with an Android device than between two STM32WB because the smartphone choose the connection interval and the CE length. The peripheral can request a new connection interval (the smartphone can accept it or not) but it can't modify the CE length. You can use ST BLE Toolbox application, that allow to do data transfer measurement (uplink and downlink).
The data throughput computation is done at GATT level.
You can look AN5604 to have more informations.
Best Regards
2022-03-21 2:27 AM
I found out the data trougput depends a LOT of the BLE chipset of the android phone/device.
My phone didnt have BLE5.0 2M high speed support.
Newer i-phones and Samsung phones/tablets would be able to archieve this data trougputs.