cancel
Showing results for 
Search instead for 
Did you mean: 

seems access to the backup domain is not granted when calling RTC_EnterInitMode() and RTC is clocked by LSI, at least on STM32WB55

LVers.1
Associate III

Recently i experimented with the RTC modules and came accross an issue where HAL_RTC_Init() fails because RTC_EnterInitMode() fail with HAL_TIMEOUT

After debugging, it seems that HAL_PWR_EnableBkUpAccess() need to be called before HAL_RTC_Init()

It appear that HAL_PWR_EnableBkUpAccess() is called if the LSE is used, but not if LSI is used. See line 775 of stm32wbxx_hal_rcc_ex.c.

Question: when is HAL_PWR_EnableBkUpAccess() supposed to be called ?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Remy ISSALYS
ST Employee

Hello,

After reset, the backup domain is protected against possible unwanted write accesses. To enable access to RCC_BDCR to select the RTC source clock and RTC registers use HAL_PWR_EnableBkUpAccess() function.

Before to perform RTC_EnterInitMode(), we need to select the RTC clock source inside RCC_BDCR using the HAL_RCCEx_PeriphCLKConfig() function and enable RTC source clock using the __HAL_RCC_RTCAPB_CLK_ENABLE() function.

To perform these actions, the driver provides the weak function HAL_RTC_MspInit() that can be overwritten by user function with same name. This function is call inside HAL_RTC_Init() function just before RTC_EnterInitMode(). This function configures the hardware resources need to access to RTC registers

If you look BLE_HeartRate project, you can see that HAL_PWR_EnableBkUpAccess() is called in SystemClock_Config() and HAL_RTC_Init() is called in MX_RTC_Init(). So HAL_PWR_EnableBkUpAccess() is called before HAL_RTC_Init() and need to be called in this order.

Best Regards

LVers.1
Associate III

Dear Remy,

Thanks a lot for taking the time to answer my question.

I agree that HAL_PWR_EnableBkUpAccess() must be called before HAL_RTC_Init(). That's clear to me.

My concern was more about why HAL_PWR_EnableBkUpAccess() is called during HAL_RCC_OscConfig() when the LSE is used. (see the call to HAL_PWR_EnableBkUpAccess() line 775 of stm32wbxx_hal_rcc_ex.c) and not when the LSI is used (LSI condfiguration is handled between lines 626 to 762 of the same stm32wbxx_hal_rcc_ex.c and there is no call to HAL_PWR_EnableBkUpAccess()).

So basically, when using LSE to clock the RTC the HAL do enable access to the backup domain, but when using the LSI to clock the RTC, the user must call HAL_PWR_EnableBkUpAccess() himself.

I checked the BLE_HeartRate project, and indeed i see the call to HAL_PWR_EnableBkUpAccess() from SystemClock_Config()  . However i don't think i can modify this SystemClock_Config() function as it is generated by stm32cubeMX.

Your suggestion to use HAL_RTC_MspInit() to call HAL_PWR_EnableBkUpAccess() is very valuable and would indeed provide an excellent solution. Thank you.

Thanks for the support

Remy ISSALYS
ST Employee

Hello,

As the LSE is in the Backup domain and write access is denied to this domain after reset, you have to enable write access using HAL_PWR_EnableBkUpAccess() function before to configure the LSE. And I suppose that LSI isn't in the Backup domain, so don't need to enable write access to this domain.

Best Regards