2022-01-18 03:30 PM
Any program that I generate using STM32CubeIDE for the STM32WB with BLE enabled hangs until I comment out the following line. What need to change in the initialization sequence?
/**
* We should never end up in this case
* However, if due to any bug in the timer server this is the case, the mistake may not impact the user.
* We could just clean the interrupt flag and get out from this unexpected interrupt
*/
while(__HAL_RTC_WAKEUPTIMER_GET_FLAG(phrtc, RTC_FLAG_WUTWF) == RESET);
2022-02-14 07:47 AM
same issue here under zigbee stack , i think it's related to clock configuration but idk what
2022-02-23 07:42 AM
Hello,
See my answer on this post:
Best Regards