cancel
Showing results for 
Search instead for 
Did you mean: 

Problem With NUCLEO F746ZG or GATEWAY RisingHF...

RVasq.4
Associate II

HI. I bought the STM32WL lora HF Package (lora getaway + lora sense)

I programmed the gateway as appear in the youtube here the link

(https://www.youtube.com/watch?v=uJU3YM1MWN4)

It worked well for 1 month, suddenly I lost the signal from the node, and I check the TTN, firmware, APPKEY, DEVKEY, etc, finally, I check the gateway and realized with the following mesage in the log.

  _/_/_/  _/_/_/  _/_/_/ _/_/_/ _/   _/  _/_/_/ _/  _/ _/_/_/

  _/  _/  _/  _/     _/  _/_/  _/ _/    _/  _/ _/

 _/_/_/   _/   _/_/   _/  _/ _/ _/ _/ _/_/ _/_/_/_/ _/_/_/

 _/  _/  _/     _/  _/  _/  _/_/ _/  _/ _/  _/ _/

_/  _/ _/_/_/ _/_/_/  _/_/_/ _/   _/  _/_/_/ _/  _/ _/

Powered by RisingHF & STMicroelectronics

-------------------------------------------------------------------------------

      VERSION: 2.1.7, Nov 6 2018

        LOG: OFF

      AT ECHO: ON

     BAUDRATE: 115200bps

      MACADDR: 08:00:27:0C:xx:xx

     ETHERNET: DHCP

       DNS1: 114.114.114.114

       DNS2: 8.8.8.8

    NTP SERVER: 1.ubuntu.pool.ntp.org

    EUI PADDING: {3, FF}, {4, FF}

    GATEWAY ID: 080027FFFF0Cxxxx

      LORAWAN: Public

  LORAWAN SERVER: router.eu.thethings.network

  UPLINK UDP PORT: 1700

 DOWNLINK UDP PORT: 1700

     CHANNEL0: 867100000, A, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL1: 867300000, A, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL2: 867500000, A, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL3: 867700000, A, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL4: 867900000, A, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL5: 868100000, B, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL6: 868300000, B, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL7: 868500000, B, SF7/SF12, BW125KHz  (LORA_MULTI_SF)

     CHANNEL8: 868300000, B, SF7, BW250KHz     (LORA_STANDARD)

     CHANNEL9: 868800000, B, 50Kbps        (FSK)

-------------------------------------------------------------------------------

Concentrator starting...

Concentrator Radio A type UNKNOWN

Concentrator Radio B type UNKNOWN

Impossible to start concentrator

Ethernet starting...

as you can see the information, RADIO A and B, doesnt appear, could be the board is fail?

well, finally, I re-upload the firmware, erasing the board, upload the .BIN data, ETC, but nothing changes.

Thanks for your help.

Ricardo

2 REPLIES 2
YBOUV.1
Senior

Hi @RVasq.4​,

Please contact your local support for replacement. Your GW seems borken.

Hi YBouV.1

I live in chile, here doesnt exist a supplier of this technology.

I bought the Dev board in USA (MOUSER)..

any way, i appreciate your answer.

Thanks

Ricardo.