cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO_LRWAN2 gateway firmware

Valter
Associate

My P-NUCLEO-LRWAN2 gateway board (F746ZG) no longer transmits data to TTN and the serial port does not respond. I think I may have loaded a firmware by mistake, where can I find the original firmware? Thanks for the support.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Valter 

It seems to me that your Gateway is broken as in this case.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
STTwo-32
ST Employee

Hello @Valter and welcome to the ST Community :smiling_face_with_smiling_eyes:.

You can download the original.bin firmware from here.

More details are available on this link.

Best Regards.

STTwo-32.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I swear I also posted original firmware in the past.

Pro Tip, save the delivered firmware before messing around and finding out..

TTN changed their implementation at some point too, which might make older versions useless / obsolete.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Tesla DeLorean wrote:

TTN changed their implementation at some point too, which might make older versions useless / obsolete.


Indeed - "TTN v3" was a couple of years ago now.

Thanks for the firmware but there is a problem and the gateway is not working. When I boot the gateway the console displays this error:

 
Concentrator starting…
Concentrator Radio A type UNKNOWN
Concentrator Radio B type UNKNOWN
Impossible to start concentrator
 
with the original firmware the message was this:
 
Concentrator starting…
Concentrator Radio A type SX1257
Concentrator Radio B type SX1257
Concentrator started (2926ms)
 
Can you help me ? Thank you in advance
Valter

Hi @Valter 

It seems to me that your Gateway is broken as in this case.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.