2021-07-15 1:46 AM
I am trying to configure Bluetooth on STM32WB5MMG Module, but iam not able to find IPCC option in CubeMX.Please help me out.
Solved! Go to Solution.
2021-07-20 1:04 AM
You can download the version 6.3.0 that is available on the ST web site today.
2021-07-16 7:33 AM
IPCC is not configurable via CubeMX. Have a look at any of the projects available in the WB package where semaphores, buffers and related interrupts used for IPCC are configured.
2021-07-16 8:17 AM
IPCC is completely managed by STM32_WPAN.
2021-07-16 8:26 AM
Like while configuring for STM32WB55 board...we get to enable IPCC in cube MX...But while configuring the same for STM32WB5MMG Module the option is not availble in cubeMX...may i know what is the issue
2021-07-16 8:37 AM
Here in the first image for STM32WB5MMG Module the option is not availble in cubeMX...but while configuring for STM32WB55 board...we get to enable IPCC in cube MX
2021-07-19 1:32 AM
What is the CubeMX version used?
2021-07-19 1:43 AM
Version used is same (Version: 6.2.1-RC2) in both the cases.
2021-07-19 2:22 AM
Indeed, the issue is confirmed with 6.2.1. This is issue is solved in version 6.3.0 that should be released very soon.
2021-07-19 2:25 AM
Thank You so much for the information
2021-07-20 1:04 AM
You can download the version 6.3.0 that is available on the ST web site today.