2025-10-21 3:08 PM
I purchased the STM32WB5MM-DK and it has an application running. When I update CUBE-MX with the patch for STM23WB5MM , there are is no examples that match the application. The training talks about the example projects but they did not come with the update. Where can I find the source project for the Dev Boards application? I work in MKS toolset
2025-10-21 4:36 PM
Hello @PStee
What is the training you are mentioning on your post? For the STM32WB5MM-DK, examples are available here on the STM32CubeWB V1.23.0 available on the ST website and can be uploaded directly using the STM32CubeMX. About the original example that came with the board, i remember that it was the BLE_HeartRate or the BLE_Sensor.
Best Regards.
II