2025-10-19 5:25 AM
Hello,
I'm having trouble getting the latest version of the STM32 VS Code Extension to work on my remote development setup. The extension works perfectly on my local Windows machine, but fails when I connect to my Linux VM via the Remote-SSH extension.
Environment:
Host OS: Windows 11
Remote OS: Ubuntu 22.04 (running in a VMware VM)
VS Code Version: 1.105.1
STM32 VS Code Extension Version: 3.6.4
Connection Method: Remote-SSH
Problems Encountered:
Cannot Create New Project: The "Create empty project" command fails to open the project creation wizard. Nothing happens.
Bundles Manager Server Unreachable: When trying to access the bundles manager for new MCUs or firmware packs, I receive a connection error. The log shows it cannot connect to the server.
What I've Tried:
The extension functions correctly on my local Windows host. I can create projects and access the bundles manager without any issues.
I have checked the network connectivity on the Ubuntu VM, and it can access the internet (ping google.com works).
I have tried reinstalling the extension on the remote host.
It seems like there might be a network-related issue specific to how the extension operates within the Remote-SSH environment. Has anyone else encountered this? Is there a known workaround or a configuration I might be missing?
Thanks for your help!
2025-10-20 7:12 AM - edited 2025-10-20 7:12 AM
@valley_exe, I just had the opportunity to give it a try.
I have been able to install STM32CubeIDE for VSCode extensions pack version 3.6.4, display the Bundle Manager table, create empty project, build and debug it fine.
In order to guide you a bit could you past here:
cube --verbose bundle list-online
cube --verbose pack sync