2024-07-28 06:54 PM
・Overview
This project involves the development of Matter devices. We encountered an issue with commissioning the device using the obtained vendor ID. Despite following the necessary steps, the commissioning process fails. Below, we detail the steps taken and request assistance in resolving the issue.
・Steps Taken
Registering the Device in the Test DCL
Registered the device for commissioning on the Test DCL.
Registered the vendor ID and device type.
Modifying CHIPProjectConfig.h
Updated CHIP_DEVICE_CONFIG_DEVICE_VENDOR_ID and CHIP_DEVICE_CONFIG_DEVICE_PRODUCT_ID in CHIPProjectConfig.h to match the information registered in the Test DCL.
Creating Matter Device Test Certificates
Followed the instructions to generate CD and DAC certificates.
Integrated the certificates into the header file.
Build and Write
Built the modified project.
Wrote the build to the device.
Commissioning
Attempted commissioning with a HomePod mini using an iPhone.
Here is the error log.
commissioning_error.log
Solved! Go to Solution.
2024-08-19 11:15 PM
I was out of office for some time, sorry for not responding sooner. Good to know you were able to solve the issue.