Skip to main content
lzhij.2
Associate II
May 16, 2023 6:50 AM UTC
Solved

The STM32CubeIDE1.12.1 can't build the B-L475E-IOT01A AWS demo.

When I build the D:\Desktop\stm32Cube\en.x-cube-aws-v1-4-2\STM32CubeExpansion_Cloud_AWS_V1.4.2\Projects\B-L475E-IOT01A , it show me the error:

d:\app\stm32cube\stm32cubeide_1.12.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: cannot use executable file '../../../../../BootLoader_OSC/2_Images_SBSFU/SW4STM32/B-L475E-IOT01_2_Images_SBSFU/Debug\se_interface_app.o' as input to a link.

Though I add the .o into to PATH, it still error. How to deal with it?
_legacyfs_online_stmicro_images_0693W00000bkAA6QAM.pngAnd the demo package is download from st.


_legacyfs_online_stmicro_images_0693W00000bkABYQA2.png

This topic has been closed for replies.
lzhij.2
lzhij.2Best answer
Associate II
May 18, 2023 2:28 PM UTC

hello, @KDJEM.1​ 

I found the solution to solved it, click the Window->preferences->STM32Cube->Toolchain Manager. My default toolchain is 10.3-2021.10, it build the project will make error, so, I install the 7-2018 or 9-2020. And set it as default, it can solved the issue, but I show a new error when compile the following:


_legacyfs_online_stmicro_images_0693W00000bkNfbQAE.pngAre there ways to solve it ?

8 replies

KDJEM.1
ST Technical Moderator
May 16, 2023 1:29 PM UTC

Hello @lzhij.2​ ,

  

The BootLoader_OSC examples in X-Cube-AWS V1.4.2 package developed with IAR, SW4STM32, Keil, but not for STM32CubeIDE.

For using STM32CubeIDE, you can follow this User manual UM2579 Migration guide from System Workbench to STM32CubeIDE.

I hope this help you!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
lzhij.2
lzhij.2Author
Associate II
May 18, 2023 2:59 AM UTC

hi, @KDJEM.1​ ​

I have tried this, but it still show the same error. And here is some requires in " B-L475E-IOT01_AWS_converter.log ":


_legacyfs_online_stmicro_images_0693W00000bkKqWQAU.pngdoes it matter ?

lzhij.2
lzhij.2Author
Associate II
May 18, 2023 3:03 AM UTC

@KDJEM.1​ 

here is the full error:

"d:\app\stm32cube\stm32cubeide_1.12.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: cannot use executable file '../../../../../BootLoader_OSC/2_Images_SBSFU/SW4STM32/B-L475E-IOT01_2_Images_SBSFU/Debug\se_interface_app.o' as input to a link"

It's the same as it was.

KDJEM.1
ST Technical Moderator
May 18, 2023 10:40 AM UTC

Hi @lzhij.2​ ,

I made some tests using STM32CubeIDE.1.12.1 version and I didn't find any issue.

Do you have reproduced it following strictly the compilation order indicated in the readme?

Could you please compile projects in the following order. This is mandatory as each project requests some objects generated by the compilation of the previous one:

 - 2_Images_SECoreBin

 - 2_Images_SBSFU

May this discussion help you!

Please let me know if the issue is solved :) .

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
lzhij.2
lzhij.2Author
Associate II
May 18, 2023 12:35 PM UTC

@KDJEM.1​ 

I did it as the readme requires, but it still did't work:loudly_crying_face: . What is your Current toolchain ? I want to change it. And I found the same error in the internet but in other product. They said it is because the SBSFU package, I don't know whether it is true.:sad_but_relieved_face:

lzhij.2
lzhij.2AuthorBest answer
Associate II
May 18, 2023 2:28 PM UTC

hello, @KDJEM.1​ 

I found the solution to solved it, click the Window->preferences->STM32Cube->Toolchain Manager. My default toolchain is 10.3-2021.10, it build the project will make error, so, I install the 7-2018 or 9-2020. And set it as default, it can solved the issue, but I show a new error when compile the following:


_legacyfs_online_stmicro_images_0693W00000bkNfbQAE.pngAre there ways to solve it ?

lzhij.2
lzhij.2Author
Associate II
May 18, 2023 2:51 PM UTC

hello, @KDJEM.1​ 

I totaly sovled all issue, about the STM32_Programmer_CLT, I just need to install an app(Programm software) from st into the path as postbuild.sh it writes(just as default path when it is installing). Then it will build successfully. Thanks a lot for your responses:smiling_face_with_smiling_eyes:

KDJEM.1
ST Technical Moderator
May 18, 2023 2:56 PM UTC

Hi @lzhij.2​ ,

Glad to know that the issue is already fixed.

Thank you for your sharing the solution :) .

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.