cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with board connection

Alexandre__Promont
Associate III

Algumas das minhas plcas quando faço a gravação do BLE não consigo comunicação com a USB do meu computador para fazer a gravação do meu firmware.

Translation: 

When I record the BLE I cannot communicate with my computer's USB to record my firmware in some boards of mine.

 

9:26:07 : UR connection mode is defined with the HWrst reset mode
09:26:07 : ST-LINK SN : 50FF6D067788545435331167
09:26:07 : ST-LINK FW : V2J45S0
09:26:07 : Board : --
09:26:07 : Voltage : 2.63V
09:26:07 : SWD freq : 4000 KHz
09:26:07 : Connect mode: Normal
09:26:07 : Reset mode : Software reset
09:26:07 : Device ID : 0x495
09:26:07 : Revision ID : Rev Y
09:26:07 : Debug in Low Power mode enabled.
09:26:07 : UPLOADING OPTION BYTES DATA ...
09:26:07 : Bank : 0x00
09:26:07 : Address : 0x58004020
09:26:07 : Size : 96 Bytes
09:26:07 : Bank : 0x01
09:26:07 : Address : 0x58004080
09:26:07 : Size : 8 Bytes
09:26:07 : UPLOADING ...
09:26:07 : Size : 4 Bytes
09:26:07 : Address : 0x58004080
09:26:07 : Read progress:
09:26:07 : Data read successfully
09:26:07 : Time elapsed during the read operation is: 00:00:00.001
09:26:07 : UPLOADING ...
09:26:07 : Size : 1024 Bytes
09:26:07 : Address : 0x8000000
09:26:07 : Read progress:
09:26:07 : Data read failed

10 REPLIES 10

I wanted to show through STM32CubeProgrammer the part of the option bytes. I have knowledge of the memory addresses for BLE and FUS. I selected the BLE file to show which one I was using. Traditionally, I flash the BLE and the BOOTLOADER through ProgrammerCLI with a script I created, as mentioned in the previous post. Currently, I haven't been flashing the FUS because I noticed that the STM32WB55 already comes with version 1.2.0.