2024-04-18 11:57 AM
Hi All,
I can import STM32WB5MM-DK Zigbee_OnOff_Server_Coord application into STM32CubeIDE and can compile and debug, however, I would like to see .ioc file to understand more clearly how to set the clock and pins etc. I wonder if there is any place I can find .ioc file for this example.
thanks,
2024-04-18 01:06 PM
Hello @YJ99 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This example is not based on a code generated from CubeMX. So it does not contain any .ioc file. If you are looking for a .ioc file on this project, i suggest you to have a look at our example tested on the P-NUCLEO-WB55 board. This example is generated using CubeMX. So, it contain a .ioc file.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-26 06:14 AM
Hi,
I bought P-Necleo-WB55 and I could see the ioc files for some application examples, however, the ioc file and code are not matching, for example the BLE_p2pClient application shows this .ioc file.
and the schematic shows many other pins are used. Why the FW code and ioc file are not matching?
thanks,
YJ
2024-05-29 03:01 AM
Hello @YJ99
the Zigbee project may be a lot different from the BLE one. Could you give more details.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.